Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi. I want to send an "int" with the HAL_UART_Transmit method. But the strange shapes that I added appear in the picture. Why could it be?
I am developing a project that has M7 processor. I want to use Segger Jlink pin which is JDTI as GPIO.I want to keep it low until I set it. But, while flashing the code to my MCU, JDTI pin becomes high until passing the hal_initialize() function. So ...
Hello!I own an STM32F769I-DISCO board which presents an external connector called "JP1" (a picture of this one is given just below) used to power the microcontroller.So, I would like to know:What is the maximum current consumption by this external co...
Hi I'm working with STM32WB5MMG-dk. The purpose is to develop BLE Gateway. The module has a custom GATT svc with 4 GATT char svc which sends and receive bytes, this data is been provided by MSP430 to STM32WB5 vice versa. So MSP430 acts as master whe...
I am trying to use SPI and DMA in a STM32H7, but it is not worling. The spi handler goes to "HAL_SPI_STATE_BUSY_TX_RX" state as soon as i call the function "HAL_SPI_TransmitReceive_DMA" and it does not do anything, it does not even generate the clock...
Hello,I am currently working with 2 Nucleo-G0B1RE board. I adapted the "FDCAN_Com_IT_2_BOARDS" from the G0C1RE-EV example.Clocks are the same, so i think the fdcan is properly setup.I changed the RX/TX pin from PD12/PD13 to PA11/PA12, and connected t...
Is there any way for chips without the Canbus peripheral to read canbus?No external chips allowedMaybe uart or bitbanging gpios?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.