STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Getting wrong value from ADC - STM32G431KBT6

Hi everyone,I'm getting weird values from ADC in a new board that I developed. It looks like it has an offset on it, but a big one.The analog signals arriving in the pins are ok. I tested with a scope. To make sure there was nothing wrong with the an...

SCTimer/PWM equivalent in STM32?

I have a circumstance where two PWM outputs are required, and they must be precisely coupled together. A number of the other big guy's LPC micros included an SCTimer/PWM (that's State Configurable Timer...) which, without too much magic, allows a fi...

DPaul.2 by Associate II
  • 3081 Views
  • 5 replies
  • 0 kudos

STM32H7 Real Time Clock - Sub Seconds

Hi,I need to get time from the RTC at a higher resolution than 1 second. I see there are two reg's that set up the thing for sub seconds, but I don't understand how to use them. I really only need tenths of seconds. I looked at the sub seconds regis...

Debugging STM32H7B3I-EVAL with ETM

Hi,I wanted to debug my STM32H7B3I-EVAL board with J-Trace Pro through ETM interface. According to the manual of STM32H7B3I-EVAL, to enable ETM, R69 must be removed to avoid conflict with the WIFI_SPI4_MISO output, and it's also recommended to remove...

0693W00000JMvdFQAT.png
JSHI.1 by Associate
  • 773 Views
  • 0 replies
  • 0 kudos

Manually include hal library files

Hello! I know that this is not a new topic, and maybe somewhere (even in this forum) someone already answered this question multiple times, but still.....I crawled the forum looking for advice about using the HAL without CUBE, because where I work th...

MFran.4 by Senior
  • 6493 Views
  • 4 replies
  • 0 kudos

How to use BNRG2A1 in low power mode with STM32F401re

I am trying to a develop application that have Temperature sensor and i want to send data to app. but when the device is not connected then i want to put BNRG2A1 in low power mode. what is the way to do that i am using X-CUBE-BLE2 software package in...

STM32F439/FMC Configuration for External DAC

Dear all,I am almost new to SMT32 world.I would like to use FMC to write to an external DAC, Analog devices AD5447. I attach datasheet for easy reference. It is 12bit, 10Msps and parallel interface.I am using Nucleo-F439ZI board and STM32CubeIDE to t...

UART transmit DMA, receive interrupt

Hello dear friends,I use F4 series MCUs. I am looking to send UART data via DMA and receive data in interrupt. How can I reach this goal? I am able to send data via DMA and receive data in interrupt, but the problem is in simultaneous use of DMA for ...

How to convert 16-bit Timer to 32-bit?

Hello everyone,I'm using 4 timers of a stm32 nucleo board to count the increments in encoder mode. 2 timers are 16 bit and 2 others are 32 bit. The increments can be between -1,000,000,000 and +1,000,000,000.With 32 bit timers, there is no problem be...

Nmo.1 by Associate III
  • 3776 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.