STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer Interrupt with DMA (ADC, SPI), non-blocking while loop?

Hi, ​I always appreciate all members here for helping beginners like me :)​I am currently working on a project using Timer and ADC+SPI with DMA.​The main timer loop is running at 40kHz, and this frequency should be strictly guaranteed.Two DMA process...

0693W00000JMUXKQA5.png 0693W00000JMUZVQA5.png
IJo.1 by Associate III
  • 3900 Views
  • 7 replies
  • 1 kudos

Resolved! STM32H7B3I-DK ADC Control register(ADC_CR) BOOST bits

I'm checking the ADC operation with STM32H7B3I-DK board.​To set adc clock frequency up to 50MHz​, i tried to change BOOST bits of ADC_CR register.​However, unlike the rm0455 document that states that bits 8 and 9 (BOOST bits region) can be set, when ...

SPark.28 by Associate II
  • 2716 Views
  • 5 replies
  • 0 kudos

Delay generator based on STM32F429

HelloI am trying to delay a 1Hz digital signal.I would like to generate a delay varying from a few microseconds to 10 ms.I tried to use ETR, TI1_ED and PWM input but I didn't manage to found out how to do.Does anyone has an idea on how to proceed?Bes...

stm32F103 ibis model error!

Error :Messages for model XXXX:Vmeas_(rising/falling) is set,It is necessary for delay neasurements. satisfy Vinh >= Vinl.

sjian by Associate
  • 1774 Views
  • 3 replies
  • 0 kudos

What happens when I read/write byte at arbitrary address shown as reserved in memory map (or write to flash memory address)?

I am exploring the memory space of my STM32F051 using a very simple hex monitor that communicates through a serial port. I can (attempt to) read/write a byte at any arbitrary address in the 32-bit address space. Within the SRAM area (starting at 0x20...

wb0gaz by Senior
  • 1839 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G4 DAC white noise

How to set up white noise in stm32g431kb DAC?​DAC works, I can produce sine wave but cant generate white noise.​​​I set DAC->CR WAVE1 to 01 (noise), DAC->CR TEN1 to 1 (trigger enable) and DAC->CR EN to 1 (enable). Tried to set also DAC->CR MAMP1 from...

oeliks by Senior
  • 2373 Views
  • 3 replies
  • 0 kudos

UART4 and UART5 Receive DMA interrupt on STM32F767ZI

I am using receive DMA to mange reception of data on UART4 and UART5.The setting of both UARTs is identical. UAERT4_RX is using DMA1 Stream 2UAERT5_RX is using DMA1 Stream 0I’m using halt transmit, transmit completed callbacks and idle interrupt to m...

MGold.1 by Associate
  • 1528 Views
  • 2 replies
  • 0 kudos

Resolved! What kind of chips can I connect to QuadSPI bus

Hello dear experts,Reading the ST literature abour QuadSpi, I noticed that they only mention the flash as available peripheral chips on the QuadSPI Ibus. i would like to increase the amount of RAM on the stm32F446RE to create a buffer when writing to...

papageno by Associate III
  • 7336 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.