2022-01-31 6:25 AM
Hey,
I create some enums and struct to declare specific pin settings. In .h file I create these struct and enums:
typedef enum {
ePin_Led_Stat=0,
ePin_Led_GPS_Fix,
ePin_USART1_Tx,
ePin_USART1_Rx,
ePin_USART2_Tx,
ePin_USART2_Rx,
ePin_Name_Last
} ePin_Name;
typedef struct {
uint32_t port;
uint32_t pin;
uint32_t mode;
uint32_t speed;
uint32_t output_type;
uint32_t pull;
uint32_t alternate;
uint32_t baudRate;
uint32_t dataWidth;
uint32_t stopBits;
uint32_t parity;
uint32_t transferDirection;
uint32_t hardwareFlowControl;
uint32_t overSampling;
} s_GPIO_Init_t;
Then in .C file I wrote this code:
s_GPIO_Init_t pin_name[] = {
[ePin_Led_Stat] = {GPIOB, LL_GPIO_PIN_5, LL_GPIO_MODE_OUTPUT, LL_GPIO_SPEED_FREQ_LOW, LL_GPIO_OUTPUT_PUSHPULL, LL_GPIO_PULL_NO, 0, 0, 0, 0, 0, 0, 0, 0},
[ePin_Led_GPS_Fix] = {GPIOB, LL_GPIO_PIN_4, LL_GPIO_MODE_OUTPUT, LL_GPIO_SPEED_FREQ_LOW, LL_GPIO_OUTPUT_PUSHPULL, LL_GPIO_PULL_NO, 0, 0, 0, 0, 0, 0, 0, 0},
[ePin_USART1_Tx] = {GPIOB, LL_GPIO_PIN_6, LL_GPIO_MODE_ALTERNATE, LL_GPIO_SPEED_FREQ_VERY_HIGH, LL_GPIO_OUTPUT_PUSHPULL, LL_GPIO_PULL_NO, LL_GPIO_AF_7, 115200, LL_USART_DATAWIDTH_8B, LL_USART_STOPBITS_1, LL_USART_PARITY_NONE, LL_USART_DIRECTION_TX_RX, LL_USART_HWCONTROL_NONE, LL_USART_OVERSAMPLING_16},
[ePin_USART1_Rx] = {GPIOB, LL_GPIO_PIN_7, LL_GPIO_MODE_ALTERNATE, LL_GPIO_SPEED_FREQ_VERY_HIGH, LL_GPIO_OUTPUT_PUSHPULL, LL_GPIO_PULL_NO, LL_GPIO_AF_7, 115200, LL_USART_DATAWIDTH_8B, LL_USART_STOPBITS_1, LL_USART_PARITY_NONE, LL_USART_DIRECTION_TX_RX, LL_USART_HWCONTROL_NONE, LL_USART_OVERSAMPLING_16},
[ePin_USART2_Tx] = {GPIOD, LL_GPIO_PIN_5, LL_GPIO_MODE_ALTERNATE, LL_GPIO_SPEED_FREQ_VERY_HIGH, LL_GPIO_OUTPUT_PUSHPULL, LL_GPIO_PULL_NO, LL_GPIO_AF_7, 115200, LL_USART_DATAWIDTH_8B, LL_USART_STOPBITS_1, LL_USART_PARITY_NONE, LL_USART_DIRECTION_TX_RX, LL_USART_HWCONTROL_NONE, LL_USART_OVERSAMPLING_16},
[ePin_USART2_Rx] = {GPIOD, LL_GPIO_PIN_6, LL_GPIO_MODE_ALTERNATE, LL_GPIO_SPEED_FREQ_VERY_HIGH, LL_GPIO_OUTPUT_PUSHPULL, LL_GPIO_PULL_NO, LL_GPIO_AF_7, 115200, LL_USART_DATAWIDTH_8B, LL_USART_STOPBITS_1, LL_USART_PARITY_NONE, LL_USART_DIRECTION_TX_RX, LL_USART_HWCONTROL_NONE, LL_USART_OVERSAMPLING_16}
};
void GPIO_Init (ePin_Name Pin) {
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_USART_InitTypeDef USART_InitStruct = {0};
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOD);
GPIO_InitStruct.Pin = pin_name[Pin].pin;
GPIO_InitStruct.Mode = pin_name[Pin].mode;
GPIO_InitStruct.Speed = pin_name[Pin].speed;
GPIO_InitStruct.OutputType = pin_name[Pin].output_type;
GPIO_InitStruct.Pull = pin_name[Pin].pull;
GPIO_InitStruct.Alternate = pin_name[Pin].alternate;
LL_GPIO_Init(pin_name[Pin].port, &GPIO_InitStruct);
if ( pin_name[Pin].alternate == LL_GPIO_AF_7 ) {
USART_InitStruct.BaudRate = pin_name[Pin].baudRate;
USART_InitStruct.DataWidth = pin_name[Pin].dataWidth;
USART_InitStruct.StopBits = pin_name[Pin].stopBits;
USART_InitStruct.Parity = pin_name[Pin].parity;
USART_InitStruct.TransferDirection = pin_name[Pin].transferDirection;
USART_InitStruct.HardwareFlowControl = pin_name[Pin].hardwareFlowControl;
USART_InitStruct.OverSampling = pin_name[Pin].overSampling;
if (Pin == 2 || Pin == 3) {
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_ConfigAsyncMode(USART1);
LL_USART_Enable(USART1);
} else {
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_ConfigAsyncMode(USART1);
LL_USART_Enable(USART1);
}
}
}
void GPIO_Set (ePin_Led led_pin) {
LL_GPIO_SetOutputPin(pin_name[led_pin].port, pin_name[led_pin].pin);
}
void GPIO_Reset (ePin_Led led_pin) {
LL_GPIO_ResetOutputPin(pin_name[led_pin].port, pin_name[led_pin].pin);
}
void GPIO_Toggle (ePin_Led led_pin) {
LL_GPIO_TogglePin(pin_name[led_pin].port, pin_name[led_pin].pin);
}
void GPIO_Read (ePin_Name Pin) {
LL_GPIO_ReadInputPort(pin_name[Pin].port);
}
As I understand the warning, I'm trying to get specific port with pin_name[Pin].port , but something isn't right with types. I also get other warnings for all functions when trying to pass this kind of port calling: passing argument 1 of 'LL_GPIO_Init' makes pointer from integer without a cast [-Wint-conversion].
Any ideas how to declare port in my struct to fix this?
Solved! Go to Solution.
2022-01-31 6:49 AM
> uint32_t port;
this should be of type GPIO_TypeDef *, not uint32_t, in order to avoid the warning.
2022-01-31 6:49 AM
> uint32_t port;
this should be of type GPIO_TypeDef *, not uint32_t, in order to avoid the warning.
2022-01-31 9:36 AM
Yeah, I managed to figure that out by myself, but thank you, this was indeed the problem :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.