STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431 SPI & DMA interrupt issue

On a STM32G431K8 I'm using the DMA1 to handle SPI1 data transfer (channel 1 for data receiption and channel 2 for data transmission).I'm using STM32CubeMX for code generation, resulting in following SPI1 and DMA1 initialization:/** * @brief SPI1 In...

0693W00000JOcKcQAL.jpg 0693W00000JOcLaQAL.jpg 0693W00000JOcQQQA1.jpg 0693W00000JOcLpQAL.jpg

STM32L562VET6Q stuck on interrupt enable

Hi,I'm working on una custom board with the STM32L562VET6Q, and i'm also using the STM32CubeIDE for developing and the STlinkV2 for debugging.I'm struggling because if any interrupt is enabled the program hang.I have made a simple configuration with ...

STM32L46 CAN : Data reception from remote problem

I am using STM32L46 CAN and trying to receive a chunk of data from the remote device .When its 73bytes I do not get any messages . I see the first 8 bytes in RDL0R and RDH0R. Also I see RF0R as 0 FIFO interrupt being enabled. I am using STM HAL APIs...

RDodd.1 by Associate II
  • 888 Views
  • 0 replies
  • 0 kudos

STM32L4 Bypass Oscillator

Hello,I am designing a circuit that needs a HSE and a LSE oscillator for USB and RTC respectively, and need to solder it by hand. Would a bypass oscillators in a SOT23-5 package (i.e. the SiT2024BA-S2-33E-8.000000G and the SIT1630AE-S6-DCC-32.768G) w...

Aaronium by Associate III
  • 1427 Views
  • 1 replies
  • 0 kudos

Transfer time when using DMA and ADC

Hi, I am using a STM32F407. I programmed one channel of ADC1 to start on the falling edge of TIM8, which has a frequency of 100 kHz. So far so good, the ADC performs a conversion every 10 us (100kHz), measured with the HAL_ADC_ConvCpltCallback functi...

0693W00000JP4HCQA1.png
LSoll.1 by Associate II
  • 3264 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.