STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it normal to have to manually press the reset button on the development boards to connect to the development boards?

Hi! I am grad student that is a newcomer to the STM32 MCU platform. I want to ask a question about the problems I have been experiencing with my development boards. Is it normal to have to manually press the reset button on the development boards to ...

0693W00000KaCn7QAF.png 0693W00000KaCnMQAV.png 0693W00000KaCoFQAV.png
jhin by Associate II
  • 4259 Views
  • 5 replies
  • 1 kudos

Resolved! BACKUP SRAM affects the other tasks

Hi,I am using backup sram in stm32f429zi. Data Read write in backup sram section is executing properly and data will retain after power down. But when we do the power UP then my program is not executing from main loop. so my code is not working as re...

ADank.2 by Associate II
  • 1847 Views
  • 2 replies
  • 0 kudos

stm32l476 a/d questions

If I am doing software trigger single conversion of 3 a/d channels and I set my end of conversion selection to be 'End of Single conversion' (CubeMX): Can I expect my to enter my ISR A/D callback at EACH EOCIF?All indications are that if I read the A...

SWenn.1 by Senior III
  • 919 Views
  • 1 replies
  • 0 kudos

STM32-HAL CAN transmits empty messages

I'm trying to transmit messages through CAN using HAL library. For test I repeated code from the first part of this video I have the same bluepill so I just did the same. Also I've tried his project, but changing Nucleo RE to ZE model. I've looked th...

0693W00000KaJJxQAN.png 0693W00000KaJKbQAN.png
LFili.2 by Associate
  • 1203 Views
  • 0 replies
  • 0 kudos

SPI Slave mode using DMA and soft NSS

I'm trying to transmit some data using DMA as a slave SPI device. I'm sending 8 byte but the peripheral always gives me 9 byte on the MISO line (first byte twice). The Master NSS is connected to a GPIO input (SPI_ENABLE) using external interrupt Mode...

0693W00000JOrukQAD.jpg
wh by Associate III
  • 6362 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.