Current consumption in stop mode 1 using STM32G0C1. Does anyone get less than 1mA?
Does anyone get good results in current consumption with STM32G0C1?I'm using stop mode 1, HSI as clock source and can't get below 1mA on current consumption.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Does anyone get good results in current consumption with STM32G0C1?I'm using stop mode 1, HSI as clock source and can't get below 1mA on current consumption.
I am using example code SPI_TwoBoards_FullDuplex_DMA, and want to change SPI1 to SPI2. LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI2);However, in the above line, compiler complains LL_APB2_GRP1_PERIPH_SPI2 not defined.I wonder why.
I am using spi slave mode,hardware nss setting.when cs is low,if there are a lot of clocks due to noise,Is shift register cleared at the rising nss edge?
Using a RTC example from the IDE, the STM32L562 discovery board gets to partly erasing the flash, before it stopsSTMicroelectronics ST-LINK GDB server. Version 6.0.0Copyright (c) 2021, STMicroelectronics. All rights reserved.Starting server with the ...
Hi ,I want to use my controller as a modbus slave. there is interrupt call back function which receive predefine data.but the modbus function like 15,16 have 10 to 11 byte of data and other function has 8 byte ,how to receive that thanking you
Hi! I'm writing to ask help about LPSDR SDRAM configuration on STM32F7.Currently I have a board with a normal SDRAM that is working fine. The design is based on the STM32F769I-DISCOVERY and it uses the MT48LC4M32B2 Micron SDRAM.The configuration is t...
I'm getting debugging Error "undefined debug reason 8 - target needs reset" with ST-Link V2, BluePill (STM32F103) & STM32CubeIDE, debugger config. is "ST-Link OpenOCD", Although STM32Programmer download & run with same ST-Link V2 without any problem....
These bits are always 0 and I can't change the voltage scaling of MCU (The code is stuck at both "while"s). The MCU P/N is STM32H743IIT6. The starting part of the code is:int main(void) { PWR->D3CR=0x0000C000; //changing voltage scaling to VOS1 ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.