STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How can I use UART manually, without HAL_UART_***() functions?

NUCLEO-H723ZG dev. kit.I need take over the full control of the USARTx. I need a TX interrupt and the RX interrupt handled manually independently the HAL_UART_*** functions. The HAL_UART_Receive_IT() and the HAL_UART_Transmit_IT() is useless for me. ...

Louie88 by Senior II
  • 3365 Views
  • 2 replies
  • 0 kudos

HAL_UART_Transmit sends extra '00' between each byte

This is probably a simple question but I can't find a reason for it - Im using the USART on a stm32L412 and I am sending 3 bytesuint16_t SendDataOn[3]={0x90,0x3C,0x3E}; HAL_UART_Transmit(&huart1,(uint8_t*)SendDataOn,3, 100)Except when I send this, I ...

deep_rune by Associate III
  • 3232 Views
  • 4 replies
  • 0 kudos

Resolved! Timer1 doesnt generate an Output while Timer3 does (STM32L552)

I am trying to use the output compare mode of TIMER1 to produce an accurate time course on the PE9 pin. For some reason I don't get an output signal on this pin. Instead, when I use TIMER3 with the same settings as TIMER1, I get an output signal on p...

FelixD by Associate
  • 2098 Views
  • 2 replies
  • 0 kudos

Don't debug. [ .elf file not found ]

hello everyone,I have the Nucleo F410RB board and I can't debug it. It gives me an error "Error message form debugger back end" and tells me that my .elf file is not found or the directory."F410RB_TEST.elf No such file or directory" The file does exi...

FGuti.1 by Associate II
  • 1576 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.