STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug in STM32CubeIDE, Version: 1.10.1, Build: 12716_20220707_0928 (UTC), regarding IRQ on DMA transfers with STM32F401

I have a small project which should generate an interrupt whenever a DMA transfer has completed. If I build the code for an STM32F411 then it works exactly as expected. If I build that same code for an STM32F401, which is within the same family as ...

SLink.1 by Associate
  • 1413 Views
  • 3 replies
  • 1 kudos

PWM with BKIN

Hello,I want to use the Timer1 CH1 and CH1N of the STM32H563ZI with dead time generator and break input functionality. It should behave in that way that when the break input (BKIN) is triggered it should goes to a predigined idle state (for CH1 low a...

CKN by Associate II
  • 736 Views
  • 3 replies
  • 0 kudos

Resolved! WWDG has no interrupt defined in STM32G474 SVD

In STM32G474.svd version 2.1 that can be download from STM32G474RE product page , WWDG peripheral has no interrupt defined but it is actually the first (0th) interrupt. Is this a mistake or there is a reason behind not defining it in the SVD ?

mete by Senior II
  • 1476 Views
  • 2 replies
  • 0 kudos

Resolved! WFI on stm32n657

 Dear all,I’m seeing unexpected behavior on an STM32N657. A timer is configured to generate an interrupt every 1 ms, and this works as expected.I would like to use WFI to stop execution and wait for that timer interrupt. I surround the WFI with the u...

Resolved! UART to interface with TMC2209-Eval Board problems

HiI have to connect an STM34 Nucleo board to a TMC2209. I have to setup a single wire UART. Only TX is connected with the TMC board.I transmitted a datagram and when I try to receive the response I get back the initial data I have e sent.Does anybody...

RPG by Senior
  • 26253 Views
  • 35 replies
  • 0 kudos

Bootload feature for stm32C013

Product: SMT32C013Issue: firmware download in bootmodeDetails:  I’ve recently started firmware development and, with community help, I’ve managed to create firmware for STM8 and several STM32 devices. Until now, I’ve always programmed the MCU using S...

zin10 by Associate II
  • 1247 Views
  • 4 replies
  • 0 kudos

Resolved! HSE is not working on STM32F411E-Discovery

I’ve just started learning STM32 and I’m currently using the STM32F411E-Discovery board. I loaded the default code provided by the Board Selector in STM32CubeIDE and was trying to get a simple LED blink working. It works fine when using the internal ...

Duc_Tran by Associate II
  • 2975 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.