STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to read multiple channels of ADC without the DAM?

Hello,I have 15ADC channel , I read the ADC channel when some external event is gnerated ,for eg when the battery is connected to one ADC channel then the interrupt gets generated then I have to read that channel , so in ADC interrupt handler I have ...

MDeva.1 by Associate II
  • 2971 Views
  • 6 replies
  • 0 kudos

Which faster CAN 2.0 vs FDCAN Classic

I have two boards, one with STM32F303 with CAN 2.0 and a new board (same electronic, only MCU is different) with STM32G474. Software is identical too, except for the CAN/FDCAN. So I had to migrate the software from CAN 2.0 to FDCAN Classic in order t...

MAmem.1 by Associate III
  • 1149 Views
  • 0 replies
  • 0 kudos

How do I restart a timer in one pulse mode after its overflow?

Maybe I am naive, but last year this code worked and now it doesn't...I have this small lab experience where I manually implement PWM to control the brightness of the LEDs on a Nucleo F767ZI board. My idea was: let's ensure that the switching of the ...

PB1 by Associate III
  • 3746 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F746-Disco I2C Touch Panel ID replying with 0x00 CMSIS-only

STM32F746-DiscoCapacitive Touch Panel FT5336STM32CubeIDE, Windows 10CMSIS-onlyI'm developing my first I2C driver for STM32F746 using CMSIS-only, and I've decided it would be great to test my I2C skills on built-in capacitive touch panel FT5336. I use...

0693W00000LwbKmQAJ.png
ilyus by Senior II
  • 3808 Views
  • 5 replies
  • 0 kudos

HAL_I2C_Slave_Transmit_IT hangs forever

Hi there,On some MCUs, I've noticed that the second call to HAL_I2C_Slave_Transmit_IT hangs forever.An example I have is on an STM32G030K6 (which doesn't seem to happen on a STM32G474RE).I have set all pins to fast to ensure that's not the issue eith...

etheory by Senior II
  • 2435 Views
  • 3 replies
  • 0 kudos

Resolved! A Variable Control of Timer Period

Hello,I want to control a timer period with a variable. The variable value is correct because I monitored it in the watch window. But the variable was not working in the timer settings. Because when I write a digit in there, it works. Is there any su...

AE104 by Senior
  • 1813 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.