STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MB1166 Touchscreen change

Hello I've been using the MB1166 display for some time, but I noticed with the latest units the I2C device has been changed from a FT6206 to the FT6306.These are means to be software compatible, however our devices do not detect the FT6306 device on ...

STM32F4 Timer count reset

htim5 has been running and I need to zero the count (CNT?).Do I need to stop, de init, init, then start?Also it seems HAL_TIM_OC_Init() is being used with HAL_TIM_Base_Start_IT(() on the same timer, TIM5. It is used to to generate interrupts with a p...

John Hite by Associate III
  • 2442 Views
  • 3 replies
  • 1 kudos

No source available for "X_function at 0x8009c8c"

HI,Actually i am integrating .a lib files into my work environment and trying to call the functions by using the .h file and i have given proper file paths and files to linker and compiler in properties of project and while compiling the i am getti...

Anil3 by Associate III
  • 869 Views
  • 1 replies
  • 1 kudos

Edge source of TIM Input Capture?

I need to measure the On and Off times of a possibly asymmetric signal. Measuring frequency is a classic TIM Input Capture function, and in this case one is tempted to set the capture for both edges. Within the ISR, however, is there a HAL approved...

DPaul.2 by Associate II
  • 4315 Views
  • 4 replies
  • 0 kudos

Resolved! I have configured 2 SPIs in DMA and I need to get callback for both SPIs (HAL_SPI_TxCpltCallback). I am able to get callback when tried individually, but simultaneously used its causes build error. Error[Li006]: duplicate definitions .

Build ErrorError[Li006]: duplicate definitions for "HAL_SPI_TxCpltCallback";void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) { HAL_GPIO_WritePin(SPIx_NSS_Port, SPIx_NSS_Pin, GPIO_PIN_SET); }I use the same in both files ?any way ? please help

JohnsAby by Associate II
  • 1663 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.