2022-06-08 7:24 PM
Working with TIM8; I have enabled one-time-pulse, set 'Channel1' to 'Output Compare CH1', set the Output Compare Channel 1 Mode to 'Active Level On Match', and Pulse to 0. I set the timer's ARR = 65535, and set the Compare Register to 20000. I have PC6 set as TIM8_CH1 Alternate function but do not see that pin toggling when I run the timer and CNT matches 20000. Any ideas on what I could be doing wrong?
Thanks!
2022-06-09 12:03 AM
2022-06-09 10:16 AM
Thanks, that did the trick!
Now I have another minor issue: I have it set to one time pulse mode, and the output pin stays high when the timer's CNT register wraps back to 0. I would like the pin to go high for the CCR1 period ( MODE 1 ) and then go low. Do I need to set the pin low manually?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.