STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why could STM32F103 flash write last so long?

Recently we have noticed in our company problems with writing information into MCU flash. It occured, that write last longer than before and 50 ms watchdog resets device during that. We had to make watchdog delay longer to 100 ms. Now the problem occ...

ROlej.1 by Associate
  • 2239 Views
  • 3 replies
  • 0 kudos

SPWF04S Module issue

I was working on the SPWFO4S wifi Module when I noticed duplicate frames data on the server.How to Avoid Duplicate Framessteps:post commandsAT+S.SOCKW=00,370\r\n"POST server linkquery message"AT+S.SOCKQ=00\rread message"AT+S.SOCKR=00observations:Foll...

MRedd.3 by Associate II
  • 982 Views
  • 0 replies
  • 0 kudos

Detect what kinda edge currently is...

Hello guys, i am using the code below (input capture mode, timer 3) because i need measure the high and low pulses, but i am not sure how to know which edge generate the interrupt, i have configured the timer with both edges, but in the interrupt cod...

RComa.1 by Associate II
  • 1740 Views
  • 2 replies
  • 0 kudos

Resolved! CAN_Error_Code doesnt really do anyting? (stm32f0xx)

Hi im trying to develop a bit of error management in my canbus driver.I noticed there is an ErrorCode inside the canbus structure. That error code could have any of these values:  But it turns out the hcan.ErrorCode is always HAL_CAN_ERROR_NONE, even...

0693W00000QKGYhQAP.png 0693W00000QKGaEQAX.png
Javier1 by Principal
  • 1648 Views
  • 3 replies
  • 0 kudos

Resolved! Dynamic exception priority change in STM32 Cortex-M4

I am using the timer interrupt and currently, it has priority 3 once I get into the ISR then I want to change the priority to 2. I have used like below but the priority not changing.NVIC->IPR[6] |= NVIC_IPR6_PRI_25 & 0x22222222;__dsb(0);In above, __d...

Harish1 by Associate III
  • 3334 Views
  • 7 replies
  • 0 kudos

I have a P-L496G-CELL02 pack with STM32L496AG MCU with LTE Cellular Expansion board. I downloaded the package FP-ATR-LTE1 and imported the package into STM32IDE. The build fails with error.

Here's the error that I get:"c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: cannot use executable file '../../../../../Boo...

IJosa.1 by Associate
  • 691 Views
  • 0 replies
  • 0 kudos

I am using NUCLEO-H723ZG and I am trying to use SPI the spi3 as SPI MASTER to the SPI SALVE device without success using DMA. I see the perfect data in the MISO line, But I unable to receive it into the "rx_buf", always "ZERO".

static void MX_SPI1_Init(void){ /* SPI3 parameter configuration*/ SpiHandle.Instance = SPI1; SpiHandle.Init.Mode = SPI_MODE_MASTER; SpiHandle.Init.Direction = SPI_DIRECTION_2LINES; SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT; SpiHandle.Init.CLK...

0693W00000QKPAFQA5.jpg
ESega.1 by Associate II
  • 885 Views
  • 0 replies
  • 0 kudos

I'm getting sporadic I2C bus errors with no terminating ACK

I'm using STM32H743 I2C1 and FW as of december 2021.I'm testing in continous loop PMBus communication (straight I2C master interface).Appr. all 8h I'm getting a sporadic bus error.A good transaction looks like:this is a register read (addr-len=1) for...

0693W00000QKNvTQAX.png 0693W00000QKNwlQAH.png
BDimk.1 by Associate II
  • 2765 Views
  • 4 replies
  • 0 kudos

STM32H743 Config JTAG PB4 As Gpio Output?

hi when i use normal configuration for define this pin(PB4 in STM32H743) as GPIO output a problem occurs in the program.This pin is connected to the JTAG port and i use only SWD mode and pull up this pin by 10k to VCC.plz help me to config this pin a...

Natali by Associate III
  • 2310 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.