STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems during stop 2 mode issue.

Hi,I created my new project follow the SubGHz Phy Ping Pong project. I want to write ADC values to FLASH for 5ms then enter stop 2 mode for 1000ms. In PWR_EnterStopMode() function, the HAL_SuspendTick() funciton is called, but my project enter stop 2...

Resolved! How to get fixed number of pulses with PWM mode on STM32f205xx

Using timer 1 for PWM cycle generationand getting proper PWM pulses using Standarad peripheral library.My requirement is to get fixed number of PWM pulses on each channel of Timer 1For this I have used one pulse mode. using HAL library able to get de...

Skada.3 by Associate III
  • 5727 Views
  • 8 replies
  • 0 kudos

NUCLEO-L073RZ, On-chip Temperature Sensor reading problem.

We are using NUCLEO-L073RZ board and configured ADC Temperature Sensor through STMCubeMX. And we used the temperature calculation formula from the section A.8.17 of RM0377 Rev 10 (STM32L0x Reference Manual)At room temperature (around 22 – 25 degree i...

Texram by Associate III
  • 2098 Views
  • 4 replies
  • 0 kudos

Can CM4 put CM7 core to sleep (or stop or halt)

I am using the template with CM7 as gated and CM4 core boot. This behavior works fine. In my application, CM4 runs on bank1 and CM7 runs on Bank 2. One sector on Bank 2 is dedicated to store application data. So CM4 tries to write to that sector, whi...

JTari.1 by Associate II
  • 1015 Views
  • 0 replies
  • 0 kudos

TIM6 Interrupt and Compiler Optimization

I have a project (for STM32L0) that use TIM6 to generate an Interrupt every 5ms and everything works perfectly both in release and debug when built wih no optimization.Then I built the same project with -Os(optimize for Size) -ffunction-section -fdat...

MVill.6 by Associate II
  • 10893 Views
  • 10 replies
  • 0 kudos

Can I measure PWM duty cycle using DMA?

I am on STM32F401 and I want to measure PWM duty cycle (PWM input) with timer 3 and a DMA channel. I'd like to have the DMA to do several measurements and then calculate the average over it. My configuration is like this:My DMA config is like this:My...

0693W00000QKukTQAT.png 0693W00000QKukdQAD.png 0693W00000QKukiQAD.png
HStee.1 by Associate II
  • 4698 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.