STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a workaround for the 'Additional reset needed after power off/on to enable connection to the BL interfaces' bootloader bug of STM32H743?

I would like to use the integrated Bootloader of the STM32H743 for updating the firmware over I2C. I don't have access to BOOT or RESET pins at the I2C master side, so my desired procedure would be:Send a command over I2C to my firmware. Once my firm...

JArwe.1 by Associate II
  • 1175 Views
  • 0 replies
  • 0 kudos

Fill Stack with watermarks without reset handler

Hello,I need to fill the stack with watermarks, but I do not have access to the assembly startup script. Usually I would do it right at the start of the reset handler, is there another way of doing this?

LHans.2 by Associate II
  • 2060 Views
  • 4 replies
  • 0 kudos

Is this a fake UART idle line?

Hello!I'm working with UART+DMA+IdleDetection. I receiving long frames of data(250-300 bytes) 250 times per second at 921600bps without HT & TC interrupt from several sensors and one Arduino, then I send them by USB . Sometimes, I receive overwritte...

0693W00000QKwfpQAD.png 0693W00000QKwgTQAT.png
SGonz.2 by Associate II
  • 4897 Views
  • 8 replies
  • 0 kudos

STM32F303xB inconstant wrong ADC measurements

I'm using the ADC to measure power grid voltage and current at 10 kHz. For most of the time the results are coherent. however, sometimes I detected some strange values colected by the ADC, differing from the measures made with an osciloscope in the a...

Strange SPI Clock Form

Hi allI have a question regarding the clock output from STM32F446VCT6 MCU.Can anyone tell me whether the clock signal looks good for you?Because for me it looks awful. The signals are measured directly on MCU pin (trace is 2 cm and is not connected t...

YDOVG.11 by Associate II
  • 9542 Views
  • 14 replies
  • 0 kudos

Resolved! USART2 works but other USARTS don't work. (STM32F446RE)

Hello,I am struggling to use multiple USARTs. I tested that USART2 works fine but I cannot get USART1 and USART3 to work. If I can't use multiple USARTs at the same time, I would like to use only USART3. However, USART3 does not work. Do I need to ch...

LCho.1 by Associate II
  • 2777 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G474 discovery kit HRTIM ISR (HRTIM1_TIMA_IRQHandler) not hit for channel set Interrupt(SETx1) and channel reset interrupt(RSTx1).

Hi,I have enabled the interrupts for channel set (SETx1) and channel reset (RSTx1) by setting bits RSTx1IE and SET1xIE. I am trying to drive the outputs to active-inactive state via software by writing to SST and RST bits of the TIMERA.Inside the TIM...

vchilapu by Associate II
  • 3217 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.