STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Any new CPUs?

When distributors have zero stock, it is hard to know about new CPUs. Are there any? Fast do it all CPUs are interesting and so are Linux CPUs.PS I am 110% happy that I didn't use any of those in my paid designs.

LMI2 by Lead
  • 2147 Views
  • 4 replies
  • 1 kudos

Resolved! Is this an error in datasheet DocID15060 Rev 7 (STM32F103x4 STM32F103x6) - regarding SPI1_SCK when SPI_REMAP = 1.

I was setting up pin assignments for a project and encountered a conflict between datasheet and reference manual. Can this be resolved?The datasheet for STM32F103x4 STM32F103x6, filename stm32f103t4.pdf, dated 6/1/2015 9:41:55 AM appears to lack an e...

wb0gaz by Senior
  • 1827 Views
  • 4 replies
  • 0 kudos

Resolved! Optical Character Recognition

Hi ST Member, Is there any specific function pack for "Optical Character Recognition"?. I have a kit STM32H747I-Disco, Planning to do some projects in character recognition. Regards,shankari.

STM32 DFSDM simultaneous sampling of 8 MEMS microphones

I am working on a project where I would like to gather PCM data from 8 MEMS microphones, and naturally I found the DFSDM peripheral interesting. The PCM data will be sent over lightpipe ADAT using a SAI but this is out of scope of this post.This is b...

0693W00000QLEStQAP.jpg
RUlstrup by Associate
  • 1086 Views
  • 0 replies
  • 0 kudos

STM32H7 UART BAUD RATE ISSUE

Hello! I'm developing application using STM32H745 with uart interface. The problem is the behaviour of uart baudrate. I configure with hal driver uart on baudrate 115200 and try echo with terminal. The problem is that sometimes i recieve wrong data ...

Iivan.1 by Associate II
  • 6291 Views
  • 7 replies
  • 0 kudos

problem with the SPI Receive DMA1 in the STM32H723ZG?

I am using the STM32H723ZG as my development board. Here I am trying to do the SPI communication. I have an example program of the same board I had tested and it is working fine but in that they have used the BDMA for the receiving side. but I need t...

Sm.2 by Associate II
  • 2248 Views
  • 2 replies
  • 0 kudos

Does HyperRAM require terminations?

I'm having trouble figuring out if an STM32H7 needs terminations for a HyperRAM memory. The memory I'm using has variable drive strength on the HyperRAM side, so I won't need terminations for RAM->MCU direction.However, I can't find any information i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.