2022-06-27 11:28 PM
Hi Team,
I am using the stm32h745zi-Q nucleo board. Here I am trying to do Transmit and receive using the SPI in Low level LL with the DMA . But I am unable to transmit the Data using the DMA.
I am attaching my code below please check and let me know any modifications in the DMA configurations.
Thanks &Regards
sm
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#ifndef HSEM_ID_0
#define HSEM_ID_0 (0U) /* HW semaphore 0*/
#endif
/* Buffer used for transmission */
uint8_t aTxBuffer[] = "Master-communication-starts";
uint8_t ubNbDataToTransmit = sizeof(aTxBuffer);
__IO uint8_t ubTransmissionComplete = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_SPI1_Init(void);
void Activate_SPI1(void);
void WaitAndCheckEndOfTransfer(void);
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
/* System interrupt init*/
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//Activate_SPI1();
MX_DMA_Init();
MX_SPI1_Init();
/* Enable the SPI1 peripheral */
Activate_SPI1();
WaitAndCheckEndOfTransfer();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_0, LL_GPIO_MODE_OUTPUT);
LL_GPIO_TogglePin(GPIOB, LL_GPIO_PIN_0);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_RCC_SetSPIClockSource(LL_RCC_SPI123_CLKSOURCE_PLL1Q);
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_DOWN;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* SPI1 DMA Init */
/* SPI1_TX Init */
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_STREAM_1, LL_DMAMUX1_REQ_SPI1_TX);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_1, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_1, LL_DMA_PRIORITY_HIGH);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_1, LL_DMA_MODE_NORMAL);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_1, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_1, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_1, LL_DMA_PDATAALIGN_BYTE);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_1, LL_DMA_MDATAALIGN_BYTE);
LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_1);
LL_DMA_ConfigAddresses(DMA1,
LL_DMA_STREAM_1,
(uint32_t)aTxBuffer, (uint32_t) &(SPI1->TXDR),
LL_DMA_GetDataTransferDirection(DMA1, LL_DMA_STREAM_1));
LL_DMA_SetDataLength(DMA1, LL_DMA_STREAM_1, ubNbDataToTransmit);
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_STREAM_1, LL_DMAMUX1_REQ_SPI1_TX);
/* SPI1 interrupt Init */
NVIC_SetPriority(SPI1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(SPI1_IRQn);
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
SPI_InitStruct.TransferDirection = LL_SPI_HALF_DUPLEX_TX;
SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_2EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV256;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 0x0;
LL_SPI_Init(SPI1, &SPI_InitStruct);
LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_EnableNSSPulseMgt(SPI1);
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void)
{
/* Init with LL driver */
/* DMA controller clock enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
/* DMA interrupt init */
/* DMA1_Stream1_IRQn interrupt configuration */
NVIC_SetPriority(DMA1_Stream1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(DMA1_Stream1_IRQn);
LL_SPI_EnableDMAReq_TX(SPI1);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_1);
LL_DMA_EnableIT_TE(DMA1, LL_DMA_STREAM_1);
}
void Activate_SPI1(void)
{
/* Enable SPI1 */
LL_SPI_Enable(SPI1);
/* Enable DMA Stream Tx */
LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_1);
/* Master transfer start */
LL_SPI_StartMasterTransfer(SPI1);
}
static void MX_GPIO_Init(void)
{
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOC);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOH);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOE);
/**/
LL_GPIO_ResetOutputPin(GPIOB, LL_GPIO_PIN_0|LL_GPIO_PIN_14);
/**/
LL_GPIO_ResetOutputPin(GPIOE, LL_GPIO_PIN_1);
/**/
GPIO_InitStruct.Pin = LL_GPIO_PIN_13;
GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/**/
GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_14;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/**/
GPIO_InitStruct.Pin = LL_GPIO_PIN_1;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
void DMA1_TransmitComplete_Callback(void)
{
/* DMA Tx transfer completed */
ubTransmissionComplete = 1;
LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_14, LL_GPIO_MODE_OUTPUT);
LL_GPIO_TogglePin(GPIOB, LL_GPIO_PIN_14);
}
void SPI_TransferError_Callback(void)
{
/* Disable DMA1 Tx Channel */
LL_DMA_DisableStream(DMA1, LL_DMA_STREAM_1);
/* Set LED1 to Blinking mode to indicate error occurs */
//LED_Blinking(LED_BLINK_ERROR);
}
/* USER CODE END 4 */
void DMA1_Stream1_IRQHandler(void)
{
if(LL_DMA_IsActiveFlag_TC1(DMA1))
{
LL_DMA_ClearFlag_TC1(DMA1);
/* Call function Transmission complete Callback */
DMA1_TransmitComplete_Callback();
}
else if(LL_DMA_IsActiveFlag_TE1(DMA1))
{
/* Call Error function */
SPI_TransferError_Callback();
}
}
void WaitAndCheckEndOfTransfer(void)
{
/* 1 - Wait end of transmission */
while (ubTransmissionComplete != 1)
{
}
/* Disable DMA1 Tx Channel */
LL_DMA_DisableStream(DMA1, LL_DMA_STREAM_1);
}
2022-07-14 1:13 AM
Hi @Sm.2 ,
For transmit and receive data using the DMA in the STM32H7, the D-Cache must be disabled. This is well explained in this article: DMA is not working on STM32H7 to resolve the problem.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.