STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f103c8t6 change ADC to GPIO and back

I have a blue pill which I wish to turn its PA0 pin to ADC mode and then back to GPIO and once again to ADC. I used the code GPIO->MODER which seems doesnt work for F103. any idea how can I do it?

Ala by Senior
  • 1624 Views
  • 2 replies
  • 0 kudos

Combined PWM mode

Hi,I'm using the combined pwm mode using STM32L431 TIM2 and noticed this information in the reference manual RM0394, page 845."When a given channel is used as combined PWM channel, its secondary channel must be configured in the opposite PWM mode (fo...

DRH by Associate III
  • 6453 Views
  • 3 replies
  • 0 kudos

NUCLEO-F411RE will not work with External 3V3 Source.

I am trying to evaluate the low-power capabilities of the STM32F411 using the Nucleo Dev Kit. I have used a simple code provided in STM SDK to toggle LED 2 at 1 second interval. LED will toggle when the board is powered by on-board USB, or 5V at VIN....

0693W00000QMTrXQAX.gif 0693W00000QMTrMQAX.png
GPann.1 by Associate II
  • 3426 Views
  • 6 replies
  • 0 kudos

Resolved! where is the QSPI CS# Pin is used QSPI library

hi,this is the first time i have used QSPI library, I have to use external flash in QSPI mode.In the data sheet it is given that, CS# pin should be low until command instruction 16bit data will pass. as shown ablove.but when executing command the ...

0693W00000QMHONQA5.png
ykn by Senior
  • 3496 Views
  • 6 replies
  • 0 kudos

STM32F429I Discovery UART5 Data receive

Hello. According to the task of my project, I connect the GY-25 sensor to the STM32F429I Discovery board. The sensor consists of a gyroscope and an accelerometer, as well as a microcontroller that processes the raw data. After processing, the built-i...

0693W00000QMWrjQAH.png
ALeut.1 by Associate II
  • 1621 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.