STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Free UART on P-L496G-CELL02 board?

We are using the P-L496G-CELL02 demo board and want to connect an external device through an UART.Is there (for example USART1) accessible for external connection? Which ports are connected to the Arduino compatible interface? Is there an UART aviabl...

MiEx13 by Associate II
  • 2080 Views
  • 4 replies
  • 0 kudos

Problem Sending CAN Message

Posted on April 15, 2018 at 23:27I am following the example code found here to send and receive CAN messages:STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Examples\CAN\CAN_Networking\SrcI can happily receive CAN messages but when I call the followi...

andy2399 by Senior
  • 11999 Views
  • 25 replies
  • 0 kudos

Hi, We are using STM32F427IIH7 for one of our project and it is out of stock now. we found an alternate part(STM32F765IIK6) for that but the new part have some additional features like VDDSDMMC and VDDUSB . Also found some diff on PDDR_ON connection.

Hi,We are using STM32F427IIH7 for one of our project and it is out of stock now. we found an alternate part(STM32F765IIK6) for that but the new part have some additional features like VDDSDMMC and VDDUSB . Also found some diff on PDDR_ON connection. ...

APm.1 by Associate
  • 1012 Views
  • 1 replies
  • 0 kudos

input configured pin to detect frequency.

I am using STM32F103C8, in which I want to use pins which are configured as digital input to detect the square wave frequency or the frequency at which the pin is reading high and low.Is it possible without Input capture direct mode?

KGaik.1 by Associate II
  • 1869 Views
  • 2 replies
  • 1 kudos

HAL_GetTick() always return 0 when i use UART

Hi, I work with STM32L562VET6Q, and when i try to comunicate with uart HAL_GetTick() fuction doesn't work because always return 0, but if i don't use uart work perfectly, What could it be due to? I try to change prioritys in NVIC interrput table but ...

slope.1 by Associate
  • 2770 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.