STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read From SD Card gets stuck in a While-Loop (Bug?)

I am working on a custom board equipped with an STM32H753 and a SD-Card connected via SDMMC 4bit wide Bus. FreeRTOS is used. HAL is generated using CubeMX and the package "STM32Cube FW_H7 V1.9.1".CubeMX generates the file sd_diskio.c and in it (line ...

SPfis.1 by Associate II
  • 2894 Views
  • 4 replies
  • 1 kudos

Strange ADC behavior

I am working in a project where I have to sample a signal with a sampling frequency of 8 kHz with the ADC. That data is send from the ADC to SRAM using DMA and then send through UART interface. I am using a "Blue pill" board (STM32F103C8T6) with a sy...

Fx14 by Associate
  • 2439 Views
  • 3 replies
  • 0 kudos

bxCAN time-triggered communication mode not supported

The errata sheet of the STM32F042 states:The time-triggered communication mode described in the reference manual is not supported. As a result, timestamp values are not available. The TTCM bit of the CAN_MCR register must be kept cleared (time-trigge...

XPach.1 by Associate
  • 1817 Views
  • 2 replies
  • 0 kudos

Crystals for the RTC and processor - STM32L496

I would like to know what load capacitance to have the Processor and RTC crystalsmade by the vendor. Typically the crystals are precision ground with a load capacitance such that when operating in the circuit the frequency will be very close to what...

TSmit.8 by Associate
  • 1311 Views
  • 1 replies
  • 0 kudos

How to get interrupt after specified number of microseconds?

My idea was simple. Set TIM to have 1MHz after prescaler. Then set ARR to the number of microseconds. So - I toggle GPIO pin each period elapsed and I can measure the time on oscilloscope.And here come troubles: for set 1us i get 2us. For 2us I get 2...

0693W00000Stu7FQAR.png
HTD by Senior III
  • 2727 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.