STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In stm32g030f6p6 I have programmed first time and I tried to dump program second time it says ": Error: Activating device KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again "how to fix

In stm32g030f6p6 I have programmed first time the code is uploaded successfully and working and I tried to dump program second time it says ": Error: Activating device KO. Please, verify the boot mode configuration and check the serial port configura...

sjana.1 by Associate II
  • 1729 Views
  • 2 replies
  • 0 kudos

Resolved! STM32- Nucleo-H755ZIQ- LED blink- SPI

Previously I wrote a program for - Nucleo-H755ZIQ in which I used SPI- UART- RTOS. After a long time, I wanna make a new stm32 project and reuse some previous function I was using correctly before. The problem is that not only those functions don't w...

0693W00000QODqWQAX.png
STork.1 by Associate III
  • 2375 Views
  • 2 replies
  • 0 kudos

Dual Port SRAM corrupted unless read after write

I have a custom board with an stm32f733zet6 and an stlink-v3mods as a programmer/debugger.Attached is a CY7C006A-20 dual port static ram which asynchronous and I'm using it without wait. I'm running 216MHz off HSI + PLLCLKI've set timing values of 1...

Zenzizen by Associate II
  • 2967 Views
  • 5 replies
  • 0 kudos

Framing error callback with dma uart channel

Hi. I have an uart managed by dma rx channel.In order to disable the error callback when a framing error comes (HAL_UART_ERROR_FE) I have comment out the line of codehuart->ErrorCode |= HAL_UART_ERROR_FE;Is there a grace way to do that, without to ed...

A problem in switching the same ADC with different channels

Hi, My purpose is to use the same ADC with different channels (one after another). I use stm32G4 with 170MHz clock speed. I want to check ADC values within a short time period. I use Baremetal. But unfortunately, I can only read one channel. it is no...

Roshan by Associate III
  • 1462 Views
  • 1 replies
  • 0 kudos

How many manufacturing heat cycles can DSP device STM32F107VCH6 withstand before it functionality/quality is compromised?

Hi, We are using DSP device STM32F107VCH6 and would like to know how many heat cycles the chip can withstand before its operation is compromised, by heat cycles we mean surface mount reflow cycles and any subsequent removal for rework / component sal...

DWebs.1 by Associate
  • 829 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.