STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC with DMA: Watchdog interrupt and DMA values

Hi everyone!I want to read 2 channels with an ADC via DMA using circular buffer. So far so good. Now I want to use a watchdog for both channels when a certain threshold is reached. However, when the watchdog is triggered and I read the values in the ...

PSmol.1 by Associate II
  • 4973 Views
  • 6 replies
  • 1 kudos

Resolved! Internal FLASH and timer1

In my STM32L496 MCU I saw that if I activate timer1(PWM channel1) is not possible to use internal flash because FLASH_SR_PGSERR go up just after initialization (Hal_Init).while, if I disable the timer (in cube) and regenerate code, flash works as exp...

M4R10 by Associate III
  • 2918 Views
  • 5 replies
  • 0 kudos

STM32G0 Lsecss issue

Hi all,I enabled LSECSSON register after select rtc clock as said from RM.I did not have any problem but if i shutdown power and power on , device used LSI as a rtc source and it cannot start LSE. Why this is happening ?

oziesin by Associate III
  • 2137 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L4: How to setup CC1IE for TIM2

I copied the code for my timer setup, and the plan was every time the capture compare was equal the CC1IF would set and I toggle the LED in the IRQHandler; however, upon loading in the code it seems the IRQHandler only gets called once to turn the LE...

KBrad.2 by Associate II
  • 2205 Views
  • 3 replies
  • 0 kudos

How to clear all pending interrupts?

I want to clear all pending interrupts in my bootloader before jumping to the user application, otherwise an interrupt will remain pending and therefore other interrupts wouldn't be triggered in the user application.After reading the Cortex-M datashe...

IJoe.1 by Associate II
  • 12068 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.