2022-09-29 1:57 AM
Hi all,
I enabled LSECSSON register after select rtc clock as said from RM.
I did not have any problem but if i shutdown power and power on , device used LSI as a rtc source and it cannot start LSE. Why this is happening ?
2022-10-02 10:29 AM
Hello @oziesin ,
Which pin of the chip are you using to start from shutdown mode ?
Imen
2022-10-02 11:41 PM
Manually, I plug off of energy pin and plug in again.
2022-10-03 1:13 AM
Hi @oziesin ,
Make sure you are well powering OFF the device.
As you know at power ON, device start from default configuration (all status/config bits at their default status), and so behaviour at each power-on should be always the same.
When you switch poweron -> poweroff, I would suggest to check that VDD goes to ‘0’ and stay enough time w/o power.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.