STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

malloc or calloc allocation on stm32. I store some strings with calloc allocation and display that strings on the api text box. strings seems to be showing static on the api text box.Outputing strings are dynamic to be display on api text box.

Its the same strings showing on api text box. It does not change. But when I debug it I can see it changing and display on api (application interface) text box. Any idea about this?

cjaya.1 by Associate II
  • 785 Views
  • 0 replies
  • 0 kudos

Resolved! CAN Communication: Baud Rate Configuration

Hello,I have read the reference manual but the terminology used in the .ioc file and the reference manual do not align, so I am getting confused. I am using the STM32H7B3I-EVAL evaluation board, which uses a STM32H7B3LIH6Q MCU. According to the datas...

0693W00000UoNDcQAN.png 0693W00000UoNEaQAN.png
KMew by Senior III
  • 9588 Views
  • 5 replies
  • 0 kudos

STM32F303 HAL ISR being called twice

Hello!I am writing a program in which I am controlling a ST32F303 MCUs DAC1 and DAC2, thru a USB port, via LabView. The LabView part sends a data string containing the following "1,4095". The one implicates which DAC I am trying to control(in this ca...

BČern.1 by Associate
  • 3143 Views
  • 5 replies
  • 0 kudos

Resolved! External Ram interfacing with stm32

As I have been developing a printer, therefore I need fast external ram to store all the data at once and then retrieve the data from the ram to the printer board. I have used the FIFO memory but that's not enough for the data. As I need a minimum 64...

SAMIN.1 by Associate III
  • 16148 Views
  • 5 replies
  • 0 kudos

STM32G0x0 WWDG timeout formula

Can you confirm that the formula on the RM0454 manual to calculate the wwdg timeout is wrong? Shouldn't the WDGTB[1:0] parameter be WDGTB[2:0]?Thank you

0693W00000UoQxxQAF.png
SFrig.1 by Associate
  • 1514 Views
  • 2 replies
  • 1 kudos

Resolved! Slow RTC

Hi all,I'm using STM32F429 on a custom board which is running a TFT LCD and RTC is running slow compared to the computer clock. 8MHz crystal is connected to HSE but currently, LSE is using an internal clock. My question is: Can I connect the external...

Ofaro.1 by Associate II
  • 11127 Views
  • 8 replies
  • 0 kudos

How HAL I2C slave works?

I'm trying to do I2C Slave but I totally don't understand how to implement it using HAL.I have a good record of data in Slave.But but when I use HAL_I2C_Slave_Sequential_Transmit_IT I get a HAL_BUSY error.What should I do? I looked at the examples bu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.