STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! __WFI not enter stop mode when debugging

Hi. When debugging stm32l476rgt6 on NUCLEO-64 __WFI instruction has no effect.My question is simple: is it possible to enter stop mode while debugging? I know that it is possible to stop dbg clock during clear DBG_STOP bit. But after awake debugger d...

ARa.2 by Associate II
  • 1943 Views
  • 2 replies
  • 0 kudos

Resolved! How to induce a RAM parity error?

Hello,I want to test some code (including the exception handler for parity error) that kicks in when a parity error gets detected by the micro. But how can I induce a parity error?The processor is stm32f0x8.

BGhaz.2 by Associate II
  • 1480 Views
  • 2 replies
  • 0 kudos

GPIO is disturbed by the alternate function

hello everyone,i work on stm32g071 to build a application , but i configure the PA9 for uart TX and the PA8 for the normal input that pull up by 3.3v. When start send data by the PA9 , PA8 is disturbed。But PA9 is not configured, the PA8 level is norm...

zli.2 by Associate
  • 2121 Views
  • 4 replies
  • 0 kudos

Delay function with TIM14 in nucleo G031K8

void TIM14_init(void){ RCC->APBENR2|=(1<<15); TIM14->PSC= 31; TIM14->SR=0; TIM14->CNT=0; TIM14->EGR|=(1<<0); } void TIM14_delay_us (int delay_us){ TIM14->ARR = delay_us; TIM14->CR1|= (1<<0); // counter enabled while (!((TIM14->SR)&1)); // wai...

0693W00000UoGKvQAN.png 0693W00000UoGKqQAN.png
Tommino by Senior
  • 5235 Views
  • 9 replies
  • 0 kudos

Erasing a page of flash on STM32L476RG

Hello everybody,I'm working on an STM32L476RG. For the moment, I'm using a nucleo-476RG board.I'm trying to write and read some data in the flash memory.I'm trying to write at the address : 0x080FF800 (first address of last page of the memory).I do t...

fab04 by Senior
  • 3867 Views
  • 7 replies
  • 0 kudos

Standby mode SDRAM sometime draw more power than usual.

If no SDRAM (disabled), enter standby mode always work as expected.When SDRAM enabled, sometime enter standby mode, draw 3mA more than usual.This is code to put SDRAM to self refresh mode before enter standby:````sdramState.command.CommandMode = FMC_...

Dat Tran by Senior II
  • 1968 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.