STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to connect STM32H745I-DISCO with openOCD using openOCD ?

Hello,I am not able to connect my ubuntu 20.04 laptop to a STM32H745I-DISCO board using openocd.```$ openocd -f board/stm32h745i-disco.cfgOpen On-Chip Debugger 0.11.0+dev-00450-ge67ff42de (2022-01-14-09:58)Licensed under GNU GPL v2For bug reports, re...

VLacr.1 by Associate II
  • 4502 Views
  • 3 replies
  • 0 kudos

Reading unavailable pin.

Hi,I have a program that will run on STM32G030C8 or STM32G030K8. C8 has a 48pin case, K8 - 32pin. The PC13 port is available in C8, there is no output in K8. If I read this pin in K8, it always returns 0, regardless of whether I turn on the pullup. W...

RB.3 by Associate
  • 1994 Views
  • 3 replies
  • 2 kudos

Resolved! How to clear internal SPI TX buffer in slave mode after transaction cancellation? SPI used in slave mode with DMA circular buffer.

Hello. I am using STM32F407VG controller. I have to transfer data from another device via SPI interface. STM32 SPI is used in slave mode, circular DMA enabled. Devices are connected via joint.In some cases I need to resynchronize data exchange. At th...

Resolved! Strange Issue with startup_stm32f072xb.s and stm32f0xx_it.c order?

Hello,I have a strange issue!, so my project is using cmake to build and it is in c++. Everything is working if i set the startup script (startup_stm32f072xb.s) before stm32f0xx_it.c But if i set it after stm32f0xx_it.c, than nothing happens it is li...

0693W00000SvzoNQAR.png
suads by Associate III
  • 2222 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.