STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SCK Active during CS High

I'm making use of the STM32L433 and using SPI to communicate with a LLCC68 from Semtech.I've noticed that my SCK is active after my CS goes high.Is this normal behavior?Code Snippet for SPI Write:LLCC68_StatusTypeDef spiWrite(uint8_t* data, uint8_t s...

0693W00000UokhpQAB.jpg
STayl.3 by Associate II
  • 808 Views
  • 0 replies
  • 0 kudos

STM32F070 Standby Mode (Not waking up...)

I wanted to test the wakup pin on the stm32f070f6.I have set pin PA0 to SYS_WAKUP1 and gave it the user name "WAKE". Before the user while loop I call: HAL_PWR_EnableWakeUpPin(WAKE_Pin); HAL_PWR_EnterSTANDBYMode();To enable wakeup (I thought) and put...

STM32H723 FDCAN1 AT CLASSIC MODE Not Working

FDCAN1 Settings:FDCAN_FRAME_CLASSIC;FDCAN_MODE_NORMAL;FDCAN_EXTENDED_ID;FDCAN_FILTER_MASK;TX/RX FIFO Enabled.Call Functions In sequency:MX_FDCAN1_Init(); hfdcan1.Init.NominalPrescaler = 5; hfdcan1.Init.NominalSyncJumpWidth = 3; hfdcan1.Init.NominalTi...

JYI by Associate II
  • 1649 Views
  • 1 replies
  • 0 kudos

The match interrupt on LPTIMx->CCRx is triggered when LPTIMx->CNT > LPTIM->CCRx - not on equal (=) as one might expect

On the STM32U5xx, ST decided to keep this interpretation of "match". It is present on other chips as well, see https://community.st.com/s/question/0D53W000004J0srSAC/stm32l0-lptim-generating-random-compare-match-interrupt-when-changing-compare-match-...

Resolved! STM32L031G6

I have a STM32L031G6 component in a UFQPN28 package, can I install a 3.68MHZ crystal, will it work or only in a UFQPN48 package

BPres.2 by Associate
  • 1075 Views
  • 1 replies
  • 0 kudos

Interruption, but corresponding interrupt flag is not set?

Dear community,I am having a strange problem with the STM32L431.The ADC is set up for use with both the DMA and interruption. This is to de-interleave the adc results from 2 different channels, since there was problem with interleaved ADC results whe...

0693W00000UoSQbQAN.png 0693W00000UoSQqQAN.png
ZJing by Associate III
  • 4949 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.