STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SMBUS sample code for NUCLEO L496ZG

I am unable to find any working examples for this specific board with SMBUS/PMBUS.I am also having lot's of issues converting a SMBUS project from a different board.It would be great if anyone could assist me in either getting FW specific to the boar...

RENODE emulator vs. STM32L072 - how to "complete" MCU model?

Has anyone here worked with Renode? An emulator remotely similar to QEMU, but more geared towards MCUs, esp. w.r.t. emulating peripherals.https://antmicro.com/platforms/renode/Renode does not seem to have a forum, only the github issues for their pro...

SKled.1 by Senior II
  • 4177 Views
  • 0 replies
  • 0 kudos

How to properly configure ADC injected group?

Hello, I've tried to use ADC for two Potentiometers only with injected group conversion but couldn't make it work. I'm using STM32F446RE. I couldn't find solution so I'm asking here. Previously I read their value correctly via polling and I know that...

Where can I find the relation between the OSPEEDR register different value (Low, Medium, High and Very High) and the frequency of the signals I want to use?

Hello ST Microelectronics community,I'm using a STM32H743ZI and I'm currently working on configurating properly the different I/O I want to use.To do so I need to set the set the pull up/down, open drain,etc. And also the speed mode.I could not find ...

BNord.1 by Associate III
  • 3567 Views
  • 4 replies
  • 2 kudos

STM32l073RZ dual boot, bank 2 not work.

Dear.I work with stm32l073RZ and I have a blinking led code and that code works on bank1, but it doesn't work on bank2. The strangest thing is that I also used the sample code for a flashing led from stmcubel0 and it worked. I think it may be because...

About the calibration of the ADC on STM32H747

I am currently trying on the linearity calibration and I am following the protocol (down below) but I do not understand where I am supposed to get the saved linearity correction factor bits[159:150] (step 3)? Every single ADC register is 32 bits at m...

0693W00000Nt33eQAB.png
HTess.1 by Associate III
  • 1201 Views
  • 1 replies
  • 0 kudos

STM32F412R HSI clock calibration with LSE

Hello,I'm looking for a way to calibrate HSI by using LSE. I've found some documents that describes the way. My situation is a little bit tough. I can't change PCB and I can't draw a way from LSE to TIM5 - channel 4. I'm looking for a way which will ...

OOzka.1 by Associate
  • 766 Views
  • 0 replies
  • 0 kudos

I use STM32H735 and her backup memory at 0x3880_0000 (4KB). All works OK if I use SCB_CleanDCache_by_Addr(0x38800000, 4096) after a write. Is it possible to disable dcache in this area ?

I tried to configure MPU using standard configuration generated.I tried this codeMPU_Region_InitTypeDef MPU_InitStruct;   HAL_MPU_Disable();   /* Configure the MPU as Strongly ordered for not defined regions */ MPU_InitStruct.Enable = MPU_REGION_ENAB...

PMina.2 by Associate
  • 911 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.