STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G4 Timer Update Triggered ADC Conversions Issue

Hi ;I'm trying to configure the ADC1 and ADC2 modules to get them triggered via tim1_trgo2 for a dual simultaneous regular conversion start but no success until now .Before I tried to do this I verified that I can succesfully trigger these modules ov...

BG1 by Senior
  • 3460 Views
  • 4 replies
  • 2 kudos

AIS2DW12 and SMT32L0 high current

Hello everyone,board consume too much energy when the acc wakeup and start to measure the tilt.in Stop Mode : 5 uAin Wake up : 280 uAMCU setting for INT pin belong to acc : No pull up-down and rising-edge triggerfor CS pin push-pull and no pull up-do...

Zek_De by Senior
  • 1628 Views
  • 2 replies
  • 1 kudos

ASK FOR A HELP

Dear TeamWhere the technology was originally invented? about this part: STM32F437IIH6TR

SWang.14 by Associate II
  • 2699 Views
  • 5 replies
  • 0 kudos

STM32L4A6 config WKUP pin to low level trigger fail

Hi all,​I wan to use WKUP pin exit standby​ mode for low level trigger.I set WKUP pin with low level polarity in HAL_PWR_EnableWakeUpPin() function and pull-up WKUP pin.but the MCU alway wake-up when enter standby mode.​When set ​WKUP pin with high l...

WWU.807 by Associate II
  • 2523 Views
  • 3 replies
  • 0 kudos

Resolved! Using STM32F723 I2C with multiple slaves at different voltages

Dear ST Microelectronics Team,I want to connect a STM32F723IE with I2C as master, which is powered with 3.0V, to a bus with one slave with 3.0V and to another slave with 3.8V. From the datasheet I can see that the GPIOs are 5V compliant, but can the ...

Rookie38 by Associate III
  • 1811 Views
  • 2 replies
  • 0 kudos

External crystal not oscillating

Hello,I have custom board. I am working on STM32H7 controller. We use the external crystal of 25Mhz. But when we use that external oscillator using the HSE ,it doesn't provide the clock to controller. Why these happening. Can you please help me

MDeva.1 by Associate II
  • 6821 Views
  • 10 replies
  • 0 kudos

STM32H750 and SDRAM signal groups

Need your advice. PCB routing. I have Divided signals into 4 groups + (CLK) : 1: Address: SDRAM_BA[0-1]/SDRAM_A[0-11] 2: Command: SDNRAS/SDNCAS/SDNWE 3: Control: NE0/CKE0/NBL[0-1] 4: Data: SDRAM_D[0-7] ( sub goup1 ) & [8-15] ( sub group 2) 5: SD...

BHell.1 by Associate II
  • 1348 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.