STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeIDE adding code to main.c - code disappears

Is there a rule where to put code into main.c so that it stays there permanently? It happended to me now a couple of times that I added an interrupt callback function which suddenly disappeared. Are there areas in main.c where to safely put those?

Why would UART_TX need to be set as OC with external pullup, if UART is set to single-wire half-duplex mode?

 Why?What happens if the respective pin is set as Push-Pull? And what happens if only the internal pullup is enabled and there's no external pullup?And there's no point to tell that the pin has to be set as "alternate function" - of course. That ST c...

0693W00000WHa5EQAT.png

Resolved! HAL_FLASH_Program trigger error 0x40 (FLASH_FLAG_SIZERR)

STM32G473CCT uses the HAL library for writing flash pages.i have constructed some code to use the last FLASH page as NV memory.bool eeprom_write8(uint16_t address, uint8_t data) { return eeprom_write(address, &data, 1); }   bool eeprom_write(uint16_...

0693W00000WHbqWQAT.png 0693W00000WHbt0QAD.png 0693W00000WHbsHQAT.png 0693W00000WHbs2QAD.png
sde c.1 by Senior II
  • 1594 Views
  • 1 replies
  • 0 kudos

Resolved! OTP size for STM32F746XX

I found a strange mismatch in the reference manual for the OTP memory size:Accordingly to the manual page 78 (https://www.st.com/resource/en/reference_manual/rm0385-stm32f75xxx-and-stm32f74xxx-advanced-armbased-32bit-mcus-stmicroelectronics.pdf) the ...

0693W00000WHcdNQAT.png
grmpyc8 by Associate
  • 1955 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.