STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to implement SPR PPS Mode for the STM32F072 ?

Hi, I am using an NUCLEO-F072RB Board with an STUSB1602 Type-C Controller Expansion Board. My Goal is to program a Sink application which is able to use the PPS Mode. Furthermore I am using the STM32_MB1303_SNK_ONLY Project as a reference. My Questio...

SKaiba by Associate
  • 881 Views
  • 0 replies
  • 0 kudos

Resolved! Flash Programming Error Even if Flash was erased.

Hi guys,I am using and STM32L552ZET6 and I get a behavior I can not exaplain. The device is power at 1.8V in case it matters. So to put it shortly I have 2 blocks of 8 pages each. At first start I erase both of the blocks and write only in block 1 so...

CDan.1 by Associate II
  • 4029 Views
  • 3 replies
  • 0 kudos

CPU test bug in the X-CUBE-STL (gcc)

Hi, this isn't really a question, but I figured I'd share back with the community (and hopefully bring the change back into ST's next release) on the X-CUBE-STL CPU test code.There are some instances, where the APSR has some bit set in what ARM docum...

TK.0 by Associate
  • 2038 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F429ZI interface to GEN4-FT813-CTP-CLB:

Everyone, Posting for the first time here. We've been working with a 4d display that's based on an FT813 IC. The issue that we came to so far is the following.0x7C during Initialization is never detected although, it is detected from MISO. This is re...

0693W00000HnkROQAZ.png

STM32H743XIH6 芯片背�?�有水�?�,有划痕,请问是原厂工艺问题导致的�?�? 是原厂出厂就存在的�?�?

STM32H743XIH6  芯片背�?�有水�?�,有划痕,请问是原厂工艺问题导致的�?�? 是原厂出厂就存在的�?�?平时是真空�?存的,今天拆包�?��?�现有上�?�两�?情况,请帮忙解答�?

0693W00000WINQ1QAP.jpg 0693W00000WINQaQAP.png
满陈.1 by Associate
  • 990 Views
  • 1 replies
  • 0 kudos

How to manage 2 channel PWM with DMA - STM32L073

We try to generate audio signal with 2 PWM signals. We use TIM2_CH1 and TIM2_CH2 with DMA1 channel 5 and channel 3. This two PWM signals must be synchronized, but we noticed some delay between this 2 channels, which unfortunately is not constant. For...

mrasz.1 by Associate
  • 1366 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.