STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC getvalue() not giving values

Hello,I am using STM32L011G4U7 and wants to get the adc value where it showed once and not it is giving 0 for the adc raw values. Also please let me know that in order to read the vcc that is 3.3 volts do I need to select VREFINT channel as well alon...

RWagh.2 by Associate II
  • 3935 Views
  • 5 replies
  • 0 kudos

Transmitted UART message mixed with other message

I'm trying to filter bunch of NMEA message$GNGSA,A,1,,,,,,,,,,,,,99.0,99.0,99.0*1E $GPGLL,0745.76471,S,11023.30874,E,040509.000,V,N*58 $PSTMCPU,27.96,-1,98*49 $GPRMC,040510.000,V,0745.76471,S,11023.30874,E,,,061222,,,N*62 $GPGGA,040510.000,0745.76471...

AFidi.1 by Associate II
  • 1452 Views
  • 4 replies
  • 0 kudos

STM32U585 Flash overwrite

Hi, I used to write bytes at 0 in flash bytes that are erased (0xFF) but this is no more possible in the flash of the STM32U585 because of ECC that protects 16 bytes chunks I suppose.However now I have an 8K sector programmed with some data except f...

BRaff by Associate
  • 1203 Views
  • 1 replies
  • 0 kudos

Issue on I2C HAL generated by CubeMX

Hello,I think that I found an issue in the HAL code generated by CubeMx 6.6.1 with STM32L4.I2C HAL in file stm32l4xx_hal_i2c.c line 6855 there is an infinite loop :     while (__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == RESET)     {      /* Check for...

Resolved! XiP STM32H750 changing flash latency for HAL_RCC_ClockConfig

Hi, on my board i`m running bootloader in internal flash of stm32h750 together with 2 QSPI NOR chips that store main program.Bootloader starts and jumps to main program in QSPI, howeverit get`s tricky when this function is called:SystemClock_Config()...

KKiec.1 by Associate II
  • 3924 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.