STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to r/w data on flash via spi/qspi?

I want to read and write data from Flash via spi. I try some tutorial, He tell me to config and use some library.I do it but it don't work. MCU:STM32L496ZGT6Flash: S25FL128LAGMFB010

JThas.1 by Associate II
  • 2579 Views
  • 5 replies
  • 0 kudos

TRGO Timer1 to ITR0 Timer 15? Nucleo-L476

I am trying to Trigger timer 15 from timer 1....Yellow in scope pic shows timer 1 output to be used as gated trigger... I am trying to get PWM gated out of Timer 15....Can anyone tell me what I am doing wrong in the code bcz I get no PWM out of PA2?...

0693W00000Y7RgOQAV.jpg
SWenn.1 by Senior III
  • 1948 Views
  • 5 replies
  • 0 kudos

STM32H745 Can't get temperature

I've made several attempts to get the temperature from the ADC and all end up resulting in negative numbers.I'm using an ADC reference IC that provides a 2.048 reference.I've tried a few different approaches.The simplest approach I've done is trying ...

Problem with spi full duplex

in my application I use stm32F407G-DISC1 as a slave. I want to use the board the spi slave full duplexes. the problem is on the first Receive I get all the data from the master then I send data and works but the second time I only get zeros even thou...

0693W00000Y7jQ9QAJ.png 0693W00000Y7jQYQAZ.png
MAgou.1 by Associate
  • 1144 Views
  • 1 replies
  • 0 kudos

EEPROM on STM32F407 Discovery

I would like to write and read into the EEPROM of the STM32F407 Discovery, but I can't figure out which section of the Reference Manual to look at.First of all, is there an EEPROM on the F407 Discover?If so, in which section/document can I find it?Sh...

luke514 by Senior
  • 2065 Views
  • 2 replies
  • 0 kudos

Resolved! How to report bug for CubeMX generated code?

I found some bugs in the CubeMX generated code.Does it forget reset the `state` after SDIO DMA TX? when I query the TX state by `HAL_SD_GetState` always get wrong result. Dose SDIO DMA mode forget clear the transition state to SD card? when erase the...

0693W00000Y7duXQAR.png 0693W00000Y7dumQAB.png 0693W00000Y7dv6QAB.png
One by Associate
  • 2014 Views
  • 3 replies
  • 1 kudos

Resolved! How to boot on RSS?

I have STM32F407VG board and it has error in flashing time see screen. I have STM32F407VG board, and it has error in flashing time see screen. Yesterday was everything ok but today is broken, I don't know why!I found a solution https://community.st.c...

0693W00000Y7eC7QAJ.png 0693W00000Y7eC2QAJ.png
DK.7 by Senior
  • 2230 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.