STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to implement Stm32f0 output compare

This is my code. It must be generete output compare interrupt when UPEventCount == DelayloopCount then, TIM_IT_CCR2 interrupt must be occur when CNT = my value. But CCR2 interrupt occur before CNT not reach my value. I looked for a long time but coul...

jsaun by Associate II
  • 2577 Views
  • 4 replies
  • 0 kudos

Resolved! I2C4 does not work using the STM32H745 Discovery Kit

I am trying to use I2C4 Pins PD12 (SCL/D15) and PD13 (SDA/D14) but cannot get it to work. I used CubeMX to generate my project. Also, I am using the Cortex M7 for the I2C4 connections. Please tell me how I can get I2C4 to work with the  STM32H745 Dis...

BGibs by Associate II
  • 2185 Views
  • 3 replies
  • 0 kudos

Resolved! How to use all RAM regions (SRAM1/SRAM2/CCMDATARAM)

Hi, I am working with STM32F407VETx and it has total 192kb RAM, but its split into 3 regions:#define SRAM1_BASE 0x20000000UL // SRAM1(112 KB) #define SRAM2_BASE 0x2001C000UL // SRAM2(16 KB) #define CCMDATARAM_BASE 0x10000000UL // CCM(core c...

0693W00000YA0E4QAL.png 0693W00000Y8qzDQAR.png
JBond.1 by Senior II
  • 3138 Views
  • 2 replies
  • 1 kudos

Cortex-M33 instruction cycle counts?

Hello,I am looking for a list of cycle counts for each instruction in the Cortex-M33 processor. For the Cortex-M4 processor, the ARM Technical Reference Manual includes a table of cycle counts for each instruction. The M7 ARM TRM doesn't seem to ha...

How to convert temperature sensor to C?

I'm trying to read the built-in temperature sensor on the MCU we're using (STM32L011F4P6)We only have the one calibration datapoint, so I can't use the temperature conversion function I'm familiar with.The code is as follows:int32_t analog_get_temper...

SWD interface not working on STM32G0B1

Hello, I have two custom boards based on the STM32G0B1CBU. When I try to program them via the SWD interface (using ST-LINK or SEGGER J-Link), I get the "No Device Found on Target" error. I checked the schematics and used an oscilloscope to make sure ...

REist.1 by Associate II
  • 5728 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.