STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Etablish an Ethernet connection with STM32F107

Hello I wan't to use the ethernet of my MCU (STM32F107VCT6) with using Lwip module. I'm using a dev board (EasyMx Pro V7). For the moment I've connect a etehernet cable between my computer and my ethernet board I've used some example of ethernet exam...

Romano1 by Associate III
  • 4332 Views
  • 7 replies
  • 1 kudos

Resolved! How does the Error Correction Code(ECC) for FLASH memory work?

Hi! all experts in Community ST,I have been working on the embedded flash memory of STM32G474RE and the whole programming process of the flash memory has been successful.However, I do not understand how the Error Correction Code works.Referring to th...

0693W00000YAmzXQAT.png 0693W00000YAn2MQAT.png
IJo.1 by Associate III
  • 7582 Views
  • 3 replies
  • 0 kudos

So, what to expect from the 'C0?

As said, the 'C0 is mostly a cut-down 'G0. Let's now put aside the "is it a true STM8 replacement" and the price-related discussion, let's just have a look at what we can and what we can't find in these chips. I had a look at the DS and RM and here a...

STM32U585 + SAI

Dear Sir.I use ICS-43434 connected to STM32U585 through SAI.The lines of the ICS-43434 SD,SCK,WS works fine ,But when the interrupt is enabled the program crash.Attached some code frgaments.Main.c.MX_SAI1_Init();static void MX_SAI1_Init(void){ /* USE...

Resolved! STM32G030C8T6

Is STM32G030C8T6   a 10-year life commitment? How long does it live?

xwang.6 by Associate III
  • 1848 Views
  • 2 replies
  • 1 kudos

HAL_SPI_Receive_DMA() won't start a transfer in a CubeMX project that I cloned. No activity on SPI bus. HAL call returns success. .IOC and generated files all compare successfully. (only changed some GPIO, SPI is configured same) What could I be missing ?

I simply wanted to make an identical program but with a different GPIO pinout. The SPI busses are all on the same pins and configured the same. What could I have touched that would cause the SPI transfer to not start ? I had to switch to HAL_SPI_Re...

Caveman by Associate II
  • 2116 Views
  • 4 replies
  • 0 kudos

UART2 Output Stripped - NUCLEO-F401RE

Working on a prototype and am using HAL_UART_Transmit to output to UART2. Upon output over UART2 the string seems to be truncated. Code below:```char stuff[] = "HELLO YOU FINE FELLOW";HAL_UART_Transmit(&huart2,stuff,sizeof(stuff),1);```Output is HELL...

Ghomi.1 by Associate
  • 1652 Views
  • 4 replies
  • 0 kudos

MAX3232 Stops Translating When STM32L0 Running

I'm trying to interface a L0538 Discovery board to a simple TTL-to-RS232 converter board that uses a MAX3232 IC (off-the-shelf from Amazon). I have VCC, GND and TX/RX from the Discovery board (UART1) wired to the converter board. I used Cube to set u...

nobbyv77 by Associate II
  • 1139 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.