STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Initialize SDRAM in SystemInit

Hello,I am using a STM32H7A3 and a SDRAM MT48LC8M16A2P.In a project using the emWin graphic library, I would want to store the relative buffer 'aMemory' in SDRAM.By reading on community and seeing the examples I understood that I have to write a Syst...

Cannot post comment in my case

I have a case open in my profile due to technical issue with one disco board and the ST employees are updating me on the situation. I would like to reply to them but I keep getting an error whenever I try to post a comment.See screenshot for referenc...

0693W00000aJKtwQAG.png

Trying to use PWM to toggle LED, won't output to LED

Hi folks​New to STM32 and getting into it by starting with clocks, timers and ADC. All I want to do is dim a few of the onboard LED's with a pot on a breadboard. Stepping through debug I've found the following Analog input is reading values from the ...

SG.121 by Associate II
  • 5540 Views
  • 8 replies
  • 0 kudos

In STM32L562VET6Q Microcontroller in that my question is how to configure/map SRAM 2 memory address as 0x2003 0000, so , i can use it as contiguous memory of both SRAM 1 and SRAM 2 i need big size continuous memory block.

"64 Kbytes located at address 0x0A03 0000 with hardware parity check (SRAM2). This memory is also mapped at address 0x2003 0000 offering a contiguous address space with the SRAM1"

sra by Associate II
  • 1261 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.