STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Code works only in Debug Mode

The code runs in debug mode, however when I disconnect debugger and run the code normally it does not work as working in debug mode?I am using STM32H7xx single core microcontroller.Awaiting to hearing from you.

DPila.1 by Associate II
  • 7164 Views
  • 6 replies
  • 0 kudos

Resolved! The first letter isn't sent correctly in SPI.

Hello.Transmission from the master in full-duplex mode is possible, but when transmitted from the slave, only the first character is not transmitted correctly.The signal was misaligned for the first letter, what is the cause?STM32G431 NucleoSPI2 sett...

0693W00000bhGZqQAM.png 0693W00000bhGaOQAU.png 0693W00000bhGbHQAU.png 0693W00000bhGcKQAU.png
TKawa.9 by Associate II
  • 4391 Views
  • 8 replies
  • 0 kudos

Resolved! stm32g474 can bus off recovery?

1. Terminal setting: classic can, silent mode, 250kbps, commercial vehicle, stm32g4742. Symptom: There is no problem during the test, but sometimes a problem occurs with the vehicle, probably because of a can error. Symptoms not reproduced.3. Inquiri...

hyuk.1 by Associate II
  • 3570 Views
  • 1 replies
  • 1 kudos

ADC with DMA's interrupt not working on STM32F303RBT

Hi all; I am using SM32f303RBT6 with Cube version 6.21 and IAR version 9.30.I used 2 ADC unit with DMA and used one timer(TI M 4) as trigger.there are 3 other timer in code that was used as two pulsers and to make sure the number of the pulses are 1...

atavo.11 by Associate
  • 961 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.