2023-04-04 12:28 AM
1. Terminal setting: classic can, silent mode, 250kbps, commercial vehicle, stm32g474
2. Symptom: There is no problem during the test, but sometimes a problem occurs with the vehicle, probably because of a can error. Symptoms not reproduced.
3. Inquiries:
-. Can our terminal affect the external can bus in silent mode?
-. How to perform recovery in firmware when can bus off occurs?
Solved! Go to Solution.
2023-04-04 2:35 AM
Hi @hyuk.1 ,
in the silent mode (also bus monitoring mode) only recessive bits are sent to the CAN bus, so no, your terminal cannot affect the external bus.
Regarding the bus off state, your terminal should not be able to get to this state, as it is in the bus monitoring mode in which it cannot transmit any message (bus off occurs only when transmit error counter >= 255).
Anyway, the recovery sequence is described in the reference manual: "If the device goes Bus_Off, it sets CCCR.INIT of its own, stopping all bus activities. Once CCCR[INIT] has been cleared by the CPU, the device then waits for 129 occurrences of Bus Idle (129 × 11 consecutive recessive bits) before resuming normal operation."
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-04 2:35 AM
Hi @hyuk.1 ,
in the silent mode (also bus monitoring mode) only recessive bits are sent to the CAN bus, so no, your terminal cannot affect the external bus.
Regarding the bus off state, your terminal should not be able to get to this state, as it is in the bus monitoring mode in which it cannot transmit any message (bus off occurs only when transmit error counter >= 255).
Anyway, the recovery sequence is described in the reference manual: "If the device goes Bus_Off, it sets CCCR.INIT of its own, stopping all bus activities. Once CCCR[INIT] has been cleared by the CPU, the device then waits for 129 occurrences of Bus Idle (129 × 11 consecutive recessive bits) before resuming normal operation."
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.