STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

High sampling rate with ADC and no DMA

Hello All,I have some questions regarding the ADC of the STM32G071RBT6. Technically we can reach a conversion time of 400 ns if we use the internal ADC clock (35 MHz) and a sampling time of 1.5 cyc. OK, that's pretty good idealy.I am running my micro...

izamfx by Associate
  • 1906 Views
  • 2 replies
  • 0 kudos

Resolved! Data coherency with DMA and I2S audio on STM32H7

Moving from a audio effect prototype based on the STM32F407 to the STM32H757. Did a lot of stuff on the F4 with audio but on the H7 I'm getting stuck and can't get a simple audio loopback with DMA. I'm using Cirrus Logic's CS5343 and CS4344 as extern...

Alefal by Associate III
  • 14247 Views
  • 18 replies
  • 1 kudos

How to use LPTIM_TimeOut for a simple one-shot delay ?

I'm trying to realize some simple timings/delays in my application using the LPTIM, and although most of it is working, I don't understand it 100%.So the LPTIM is set up to run on the LSE clock (32768 Hz) (with a prescaler of 16, so the LPTIM is runn...

Strooom by Senior
  • 7710 Views
  • 3 replies
  • 0 kudos

What MCUs have backup SRAM maintained by VBAT?

STM32F407VG has 4kB of backup SRAM that's preserved when VDD is removed if VBAT is present. A few other MCUs in the STM32F40x line have that feature too.Do any MCUs outside of the STM32F40x line have SRAM that's preserved with VBAT? Is there a way ...

SOtte.602 by Associate II
  • 1298 Views
  • 1 replies
  • 0 kudos

Resolved! Specific format for an SFI image, specifically how to decrypt it.

We;re looking at using SFI as part of the manufacturing for a product based on STM32U5. One of the concerns we have is that STM32TrustedPackageCreator only supports a bare (not big-iron HSM) protected. One of the simplest ways for us to accomplish ...

msj by Associate II
  • 1713 Views
  • 1 replies
  • 0 kudos

erase_init.Page = 11; bricks STM32G030

I have been attempting to write to flash on an stm32G030 and manually changed the erase_init.Page = address & ~(FLASH_PAGE_SIZE - 1); to erase_init.Page = 11; and this bricked the device and is no longer able to be connected to an STlink is there any...

PGood.1 by Associate II
  • 1595 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.