2023-04-11 5:55 AM
I'm trying to realize some simple timings/delays in my application using the LPTIM, and although most of it is working, I don't understand it 100%.
So the LPTIM is set up to run on the LSE clock (32768 Hz) (with a prescaler of 16, so the LPTIM is running at 2048 Hz)
To start a delay there is this HAL function :
HAL_LPTIM_TimeOut_Start_IT(&lptim1, uint32_t Period, uint32_t Timeout)
but why are there 2 parameters ?
If I set Timeout to (eg). 2048, I get the LPTIM interrupt one second later.
But what is Period doing ? What value should it be set in this simple case ?
If I set Period to (eg) 2048 as well, I observed that the first time, I get 2 interrupts, io 1...
Also I found that the timer after expiring, is restarted automatically, so I have to stop it. Would it be possible to start it as a one-shot timer, so it expires automatically ?
It all seemed like a simple application of LPTIM, but I could not find how to do it in the HAL docs not in the forums..
Thanks.
2023-04-12 12:57 AM
I think I found a solution in the following way :
Using HAL_LPTIM_SetOnce_Start_IT() to start the timer. It still has two parameters, but I set the 'Period' to 0xFFFF and the 'Pulse' to the timeout time wanted.
Then this generates 2 interrupts : compareMatch and reload, but by adding only HAL_LPTIM_CompareMatchCallback() to handle the timer expire event, it works. The other interrupt (reload) is also firing but it calls an empty HAL_LPTIM_AutoReloadMatchCallback().
I think it could be disabled with some lower level calls, but the available HAL function enables both.
2023-04-18 6:24 AM
Hi @Strooom ,
To understand more how the LPTIM Timout works, I invite you to look to:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-19 12:16 AM
Hi Amel, thanks for your help. Actually I did consult those sources, but I did not find the answer there. Those examples are all focused on using the LPTIM to generate or handle hardware signals. My need was a pure software timer, so I can put the MCU into sleep for some time, and have it wake up after that. It's basically like a HAL_Delay() but then in (ultra) low power.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.