STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why SMT32L031x UART pins do not work?

Hello, I have a custom board with a SMT32L031F6P6 on it: PA2 and PA3 USART2 channel seems not to work even if they are correctly set in the .ioc file.I have tried the same code on the NUCLEO-L031K6 board using VCP-TX and VCP-RX (PA2 e PA15) default p...

LSant.7 by Associate II
  • 2007 Views
  • 3 replies
  • 0 kudos

STM32 PWM 2 phase

i have a question my friends, i did PWM for 2 Phase, it works correct and good, but after i stop my Timer Master and Slave in order to have Delay, i mean with HAL_ TIM_PWM_STOP, doesn't work my timer slave any more, can you help me about that?Here ar...

HA.5 by Associate III
  • 2339 Views
  • 5 replies
  • 0 kudos

SM32F411, SPI slave without NSS still receives data

Hi,I have configured an SPI as receive-only slave in CubeMX and have set NSS to "Hardware input signal":From logical point of view I now would expect, that there are no SPI data received, as long as NSS stays at high.However, the CubeMX-generated cod...

_legacyfs_online_stmicro_images_0693W00000bjkvVQAQ.png
BSchm.6 by Associate III
  • 2475 Views
  • 4 replies
  • 0 kudos

Resolved! Past Online workshops

Hi all,Does anyone know if I can watch a past Online workshop called 'Easily add intelligence to your products'? I missed the scheduled one on the 4th April and would like to watch it if available.Thanks.

MHarr.8 by Associate II
  • 1594 Views
  • 2 replies
  • 0 kudos

STM32F411RE: EXTI3 interrupt does not work

Hi,when configuring PA0/EXTI0 interrupt in CubeMX, the related code works well: when PA0 pin is toggeled, the ISR is called and following up from this, the code jumps into HAL_GPIO_EXTI_Callback().But when doing the same with PA2/EXTI2 or PA3/EXTI3 t...

_legacyfs_online_stmicro_images_0693W00000bjlAaQAI.png
BSchm.6 by Associate III
  • 947 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.