STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

control SK9822 2020 LED's via SPI using Registers

HiI need to control some SK9822 2020 RGB LED's.I figured out that with the information on this website I can control them over SPI in transmitt only mode.The Problem I have now is, that I need to do it using Registers and can't use CubeMX for setting...

Lixx by Associate III
  • 2235 Views
  • 3 replies
  • 1 kudos

What is the startup time of PVD?

I want to use the PVD function of my STM32U5(but I think this applies to nearly all STM32s) to detect when my supply voltage goes over(!) a specific threshold. But it might already be there when I enable PVD. Since this means looking for a zero on PV...

OliM by Senior II
  • 2723 Views
  • 6 replies
  • 0 kudos

Flash memory size STM32F303RET6

Good morning,I need to create a shared memory space between two applications (Bootloader and Application).I am working with STM32F303RET6 MCU.I want to do this inside flash memory and not SRAM.For that reason I found many examples and codes where fun...

RCesc.1 by Associate II
  • 3479 Views
  • 2 replies
  • 0 kudos

Resolved! Squeezing a higher resolution from U575 DAC

Hello everyone! Sorry for a dumb question - I am a piano major. I want to squeeze extra 2-3 bits of the built in DAC and so I have heard that it was possible to increase a DAC resolution by adding jitter. Could please anyone share a link to some not-...

Skfir by Senior
  • 1733 Views
  • 2 replies
  • 0 kudos

removing chip cause unexplainable artifact.

I have a st chip (HT35) with the STM32H735G-DK Discovery Kit. Projects was complete and running fine. We then had to remove the OCTO SPI nor flash chip because we need access to Pe2. but after removing the chip the app froze after MX_TIM4_Init(). The...

ulao by Associate III
  • 3766 Views
  • 9 replies
  • 0 kudos

Multi-channel ADC reading in continuous mode.

Using an STM32H757-EVAL (don't use CM4) with CubeMX. Configured my ADC1 as follows:DMA is:Start the process as follows (both calls return HAL_OK):I allow the code to run for 10 seconds and break. The m_hv_status_values buffer still has the initial va...

_legacyfs_online_stmicro_images_0693W00000bjjM0QAI.png _legacyfs_online_stmicro_images_0693W00000bjjMAQAY.png _legacyfs_online_stmicro_images_0693W00000bjjMFQAY.png
Gil1 by Associate III
  • 3876 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.