STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 interface with 16x2 LCD

I have been trying to interface STM32F401RE development board with 16x2 LCD module. I have tried making my own driver file for the same. I tried changing LCD's twice but still the same, the issue is no data is visible on the LCD . I am working on 4-b...

DJ1 by Associate III
  • 10396 Views
  • 10 replies
  • 1 kudos

STM32 MCU capabilities with parallel processing

I am trying to design a modular avionics bay whereby I came across a concept called parallel processing, whereby multiple MCU's can be utilised to both increase processing capabilities, decrease power consumption of one chip, and to allow for modular...

LWebb.1 by Associate
  • 4662 Views
  • 2 replies
  • 0 kudos

STM array not being initialized properly.

I want to run some C++ code on my STM32H747I-DISCO board. I am trying to initialize 4D vector with all values as 6. (just for initialization purposes). The shape of the vector is (1,23,249,4). I have two variables s1 and v1, which store the size and ...

SMehr.2 by Associate
  • 1525 Views
  • 1 replies
  • 0 kudos

USART3 nucleo STM32F767ZI virtual com port

I have some problems to see in the serial port the message of my nucleo board, for this board I read that for USART 3 Virtual COM SB4 and SB7 most be off, and SB5 and SB6 on, for the st/link serial but nothing happens. I debug the code and all is wor...

JVele.1 by Associate
  • 1738 Views
  • 2 replies
  • 0 kudos

STM32G4 SAI Data Processing in I2S Mode

Dear STM Community,I've configured the SAI on my Nucleo-G474RE board by setting the protocol to "I2S Standard" and data size to 24 bits to communicate with an external 24 bit ADC. Further, the SAI works together with the DMA to fill the buffers. Here...

_legacyfs_online_stmicro_images_0693W00000dDQHoQAO.png
abg1984 by Associate II
  • 5756 Views
  • 5 replies
  • 0 kudos

Resolved! How do I find out, that the battery was inserted into my system? = find out the difference between power up and reset after shutdown/standby mode ( G031 )

We have a battery driven system based on STM32G031K8 and a S2-LP for RF running from a CR2032.I use the shutdown mode to keep power as low as possible. System is done by a reed contact connected to a wake up pin.We want to find out, whether the batte...

SThie.1 by Associate II
  • 2444 Views
  • 3 replies
  • 0 kudos

Resolved! BUG with STM32H723ZGT6 in SPI1 SCLK on PG11 pin (missing)

Hello,I am making SPI DAC update function, and I could not get PG11 to output SPI1 clock. While if I switch to PB3 pin, all is perfect. (this is alternate pin for SPI1)If I toggle PG11 as GPIO, I get waveform so where is no short or something simila...

_legacyfs_online_stmicro_images_0693W00000dDV6gQAG.png _legacyfs_online_stmicro_images_0693W00000dDV6lQAG.png _legacyfs_online_stmicro_images_0693W00000dDV6qQAG.png
Linas L by Senior II
  • 2801 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.