STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UARTEx_ReceiveToIdle_IT fails to initialize

Hello There,I'm using STM32H7A3 and facing a weird issue with HAL_UARTEx_ReceiveToIdle_IT() API.STM is connected to Cellular Modem via UART. When I turn on the modem via some GPIOs, initially it throws some init data. But when I call HAL_UARTEx_Recei...

KAgga.1 by Associate III
  • 2582 Views
  • 3 replies
  • 0 kudos

In MCU STM32F103RETxLQFP64, UART program stop system

To,Sir or MadamI am making a embedded system with MCU STM32F103RETxLQFP64. In this MCU pin PC10 and PC11 is multipurpose pin. I use it for UART.In project, PC10 and PC11 is used as GPIOs. I change functionality of pin. I used pin PC10 for UART4_TX an...

BL4S5I-IOT01A issue

Hello there! I am using the B-L4S5I-IOT01A board. After setting up the AWS process, I have opened tera term to configure the device. After I configured the tera term once I press the reset button on the board, no information is being displayed on the...

DDutt.3 by Associate
  • 1321 Views
  • 1 replies
  • 0 kudos

PC13/PC14/PC15 pins on the STM32F103CBT6 usage

Hello,I have a question related to the GPIOs PC13/PC14/PC15. Due to the fact that in my project I am running out of the other GPIO pins I have a question related to those pins above. I know that those pins have limitation to max 3mA sink current so d...

Resolved! HAL_FLASHEx_Erase no effect on STMF401RE

Hi. I am writing a bootlloader application that can erase, rewrite, and jump to a user application.As a starting point, I want to make sure I can erase the user application, but the erase seems to have no effect. My sector erase code is below.uint32_...

JBark.3 by Associate II
  • 1803 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo-U575 & SIM7600G

Dear,Started with the FreeRTOS example I am trying to communicate over uart with a sim7600G. I have setup my usart2. I am able to send data but the returned value contains only the data sended and no response from the sim7600G. I have tried with an e...

T.Die by Associate II
  • 2319 Views
  • 2 replies
  • 2 kudos

STM32H747I-DISC0 accidentally disable M7 boot option

HelloI am using STM32H747I-DISC0 board, and I accidentally disable M7 boot option byte through the Programmer. And now i am not able to connect to the board using the Programmer, how should i reverse this process?BRWF

CWei .1 by Associate II
  • 1479 Views
  • 1 replies
  • 0 kudos

Resolved! HRTIM repetition counter resets on stop/start but ADC Postscaler does not - is there a way to manually reset the postscaler?

Hi there!!I'm currently working on a high frequency GaN brushless motor control application using the HRTIM's complementary outputs (CHB1/2, CHE1/2, CHF1/2), with the timer in up-down counting mode, and ADC1/2/3/4 on the STM32G474RE for inline phase ...

SGree.2 by Associate II
  • 5083 Views
  • 2 replies
  • 0 kudos

SBSFU Linker script issue on STM32F746

Hi,I've been trying to implement the SBSFU package on my STM32F746 but I got some issues.I started from the STM32F769I-Discovery example given in the SBSFU package supply by ST.I'm trying to modify the memory mapping to fit my device.When I'm debuggi...

FlorianGaudon_3-1687362634439.png FlorianGaudon_4-1687362659396.png FlorianGaudon_2-1687362618747.png FlorianGaudon_5-1687362698367.png

Resolved! HAL_I2C_Mem_Read disables interrupts

Hello all,I am working on a project which is based on stm32f103cbt7 mcu.In my project i have two freeRTOS task and 2 timer interrupts and 1 uart interrupt routine.Task 1:  handles wireless communication (it reads a buffer and if buffer has some valid...

sanju by Senior
  • 4086 Views
  • 5 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.