2023-06-16 9:37 PM
Hello all,
I am working on a project which is based on stm32f103cbt7 mcu.
In my project i have two freeRTOS task and 2 timer interrupts and 1 uart interrupt routine.
Task 1: handles wireless communication (it reads a buffer and if buffer has some valid data then it takes action accordingly). Buffer for which this task checks is filled by uart interrupt, data received on uart is filled to this buffer.
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HandleRxByte(rdata); // fills task1 buffer by checking received data.
HAL_UART_Receive_IT(&huart1, &rdata, 1);
}
Task 2: this task reads some data from External RTC over I2C and write some data to SD card over SPI and read analog channels.
Here i am facing a problem that after few minutes (random time) from device power on , buffer of task 1 does not change it's content, i.e. it freezed. For few minutes it works fine , multiple packets are handled by task1 correctly but after random time buffer content stops changing.
after debugging i found that at this moment when problem rise USART1 _> CR1 -> RXNEIE bit becomes 0 , timer and systick interrupts working fine and task 2 also working fine.
only uart interrupt disables.and i think reason is that HAL_I2C_Mem_Read disables and enable interrupts. because of this it disables uart interrupt anddoesn't enable again.
Am i right or please suggest me a solution for this.
thanks in advance .
Solved! Go to Solution.
2023-06-21 8:51 AM
"still not working fine" is not very helpful. HOW is it still not working? Are you still getting to a point where the RXInt counter stops incrementing?
Because you are getting overflow errors, that means you are loosing data. So as long as that happens your code will never work. At 38400 baud you receive a byte every 260us. Since your interrupt is unable to keep up with that, perhaps your UART interrupt priority is lower than some other (very long or very frequent) interrupt? The HAL code is a bit boated, but it should be able to keep up with that baud rate (DISCLAIMER: I have never used the F1xx series and there may be limitations that I am not aware of).
The REAL fix is to stop using interrupts and use DMA in a circular buffer. See https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx for examples.
2023-06-19 9:24 AM - edited 2023-06-19 9:27 AM
Receiving byte by byte is inefficient and can cause overload. Processing your data using HandleRxByte(rdata); might also be not the best choice (if you do serial processing in this part).
It is better to use DMA for serial communication in order reduce load. ( look for HAL_UARTEx_ReceiveToIdle_DMA documentation and use circular receive buffer.)
At least try to read more than 1 byte at a time HAL_UART_Receive_IT(&huart1, &rdata, xxx); if your protocol allows this.
2023-06-20 3:07 AM
To demonstrate my problem i have created a sample project and attached its source files. here i have created two task and one uart interrupt isr.
uart receive call back just counts number of interrupt occured.
This code works fine till random time i.e. uartRxIntCnt goes to 10000 and then 0 so on repeats and both leds LD4 and LD5 toggles fine .
but after some random time uartRxIntCnt stops increasing but both leds LD4 and LD5 toggles fine means both the task are working fine. only uart interrupt stops working.
in order to work uart interrupt fine i have to remove __disable_irq(); and __enable_irq(); from task1.
You can see the complete project in attachment.
2023-06-20 10:46 AM
You don't say what CPU clock rate and UART baud rate (and I'm not taking the time to look through your project). So we can't tell how hard you are pushing the CPU. As @Johi mentioned above, processing byte-by-byte can be expensive (again, depending on your CPU clock and UART baud rates).
You also don't show a HAL_UART_ErrorCallback() implementation. It is possible (probable) that you are getting some sort of UART error (framing or overrun, for example) which is disabling the interrupt.
2023-06-20 9:19 PM - edited 2023-06-21 8:01 AM
Thank you for the reply.
CPU clock frequency is 48 Mhz and UART baud rate is 38400.
I implemented HAL_UART_ErrorCallback() as you guided , here i am getting overrun error.
void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
{
uartErrIntCnt++;
uartErrCode = huart->ErrorCode;
huart->Instance->ICR |= (1<<3); // Clear overrun error
HAL_UART_Receive_IT(&huart1, (uint8_t*)&rData, 1);
}
But it's still not working fine.
2023-06-21 8:51 AM
"still not working fine" is not very helpful. HOW is it still not working? Are you still getting to a point where the RXInt counter stops incrementing?
Because you are getting overflow errors, that means you are loosing data. So as long as that happens your code will never work. At 38400 baud you receive a byte every 260us. Since your interrupt is unable to keep up with that, perhaps your UART interrupt priority is lower than some other (very long or very frequent) interrupt? The HAL code is a bit boated, but it should be able to keep up with that baud rate (DISCLAIMER: I have never used the F1xx series and there may be limitations that I am not aware of).
The REAL fix is to stop using interrupts and use DMA in a circular buffer. See https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx for examples.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.