STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Output push-pull with pull-up or pull-down capability

The output push-pull implies either 0 or 1 - never floating. When do we use the output push-pull with pull-up or pull-down capability? What is the application for the output push-pull with pull-up or pull-down configuration?

tzk by Associate II
  • 16357 Views
  • 6 replies
  • 2 kudos

Resolved! STM32G431 - Triggered ADC and DMA

Hi. Setup is simple:TIM2 creates the ADC_EXTERNALTRIG_T2_TRGO signal, which starts ADC. ADC is configured to use DMA to transfer the data to the buffer. hadc1.Instance = ADC1;hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;hadc1.Init.Resolution ...

mrox by Associate II
  • 4160 Views
  • 5 replies
  • 0 kudos

GPIO Problem with STM32F070RB

Hello everyone,I am developing a small program with a relay which has a data, power and ground input. This is powered at 5v and I have it connected to the GPIO PA0 output.My code is as simple as creating a task with FreeRTOS as follows:void StartDefa...

JAgui.1 by Associate II
  • 3199 Views
  • 4 replies
  • 0 kudos

How to use icache and dcache in u575?

Hello everyone! I have been reading the user manual for the u575 processor and found out that there was a cache memory there. But I have absolutely no clue how does it work and how to implement its support in code. Does anyone know any article or som...

Skfir by Senior
  • 4827 Views
  • 1 replies
  • 0 kudos

SRAM2 content lost on ECC switch off and switch on again

Hi all, (STM32U575..) we have the SRAM2 ECC active on reset by the according configuration of the flash option byte. For testing purpose I switch off the ECC by using the HAL_RAMCFG_StopECC(&hramcfg_SRAM2), manipulate one cell for a one bit error and...

PScal by Associate III
  • 1524 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.