STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Multiple USB virtual com port

Hi, I would like to make a serial to usb converter. The problem is that I need to make a usb-to-32 serial port converter.I've seen that there is nothing like this on the market and not even chips that do this.What I came up with, is to use STM32s to ...

FMass.1 by Associate III
  • 5929 Views
  • 2 replies
  • 1 kudos

How to write your own DAC driver in STM32?

I was using HAL Driver for DAC, however, it turned out not to be suitable for my project because at high sampling frequency, using HAL_DAC_Setvalue() inside a timer interrupt caused problem. So i need to write my own driver for DAC. But I have no ide...

RShre.2 by Associate III
  • 7543 Views
  • 22 replies
  • 0 kudos

Resolved! STM32U585 TZEN Program Error when reset command is used

Hi @channelI am using the B-U585-IOT2A board based on STM32U585 and am configuring TZEN and checking some sample programs. i am not able to reset the board either through the push button or through the software code "NVIC_System_Reset()" and when deb...

PJose4_0-1690804143370.png PJose4_1-1690804228703.png PJose4_2-1690804321549.png PJose4_3-1690804334101.png
PJose.4 by Senior
  • 6273 Views
  • 5 replies
  • 1 kudos

STM32H723ZGT6 vs STM32H743ZIT6 P2P compatibility

Hi,I am planning to replace STM32H723ZGT6 with the STM32H743ZIT6. I am interested in the following interfaces and using the respective in numbers MII/RMII(1 no.), SPI(1 no.), UART(4 no.), I2C(4 no.), QSPI(1 no.), OSPI(1 no.). Please do let me know if...

Sandeep1 by Associate II
  • 3501 Views
  • 2 replies
  • 0 kudos

STM32H745 usart 3 not working

Hello, i need help with my stm32h745i-disco. I use usart3 in PB10 and PB11 (which is used for vcp by default in arduino pin) and i cannot send or receive any data using that, is there any settings should i check? im using default HAL_UART_Transmit an...

BAl K.1 by Associate III
  • 4093 Views
  • 7 replies
  • 0 kudos

Resolved! How to capture and save high resolution images on STM32H7?

Test Description: Receiving an image of 1280x960 through the image sensor and saving the image to external PSRAMTest Environment- MCU : stm32h753ai- Camera Module : AN0134- psram : is66wve4m16ebll-70bliCurrent situation- Create image buffer in intern...

dorawa by Associate II
  • 2966 Views
  • 1 replies
  • 0 kudos

STM32 CAN bus accepts nonmatching addresses

Hey there!I am testing the communication between 2 STM32H7 custom-made boards using CAN bus (chip: SN65HVD230).My issue is that both ends communicate (Transmit and receive) despite the configuration filter IDs (1 & 2) I am setting. I also tried to bl...

Tee by Associate II
  • 1377 Views
  • 1 replies
  • 0 kudos

How to read two adc channels in stm32 g071?

I saw a similar post here that is related to my problem. But unlike in this post, I want to read to adc channel inside a timer interrupt which has a sampling rate of 50KHz. How do I do it? I tried following this post and but adding start and stop adc...

RShre.2 by Associate III
  • 10235 Views
  • 12 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.