STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NDEBUG doesn't seem to work as expected

I'm working through some code size optimization efforts and noticed that our list file includes some calls to __assert_func. We're not using asserts in our codebase so I'm guessing one of the standard libs is using it. I checked and we have defined N...

Konami by Senior II
  • 2241 Views
  • 3 replies
  • 0 kudos

Resolved! ESD protection on JTAG and SWD

I am reading the  "Getting started with STM32U5 MCU" guie, which mentions that JTAG/SWD lines should have a 47-Ohms resistor and a 6.1V diode for ESD protection,.I am using s STLINK-V3SET to program a custom board. STLINK already includes these compo...

dhs by Senior
  • 5957 Views
  • 3 replies
  • 1 kudos

Resolved! stm32c011f6p6

I needed a help how to implement shutdown mode and wakeup from external reset in my application   while (1) { HAL_Delay(100); // MAINS INPUT Adc_Mains(); HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1,1...

meena by Associate III
  • 6907 Views
  • 8 replies
  • 1 kudos

Current sensitivity for Analog input

Hi all,I'm working with an STM32WL and I'm looking for an information I can't found. I have a voltage divider with 2 resistors to meseaure the battery voltage. I'd like to know what is the minimum current that the stm32wl can have on an analog input ...

SBaro.11 by Associate III
  • 4262 Views
  • 6 replies
  • 3 kudos

stm32h735G_DK OB PCROP DMEP can't reset (un check)

Hello everyone, i am having issues with my board, I can't load to it. I am getting data read failed when i open stm32cubeprogrammer the OB PCROP DMEP box is checked (I did it) and I can't find a way to uncheck it. I have tried the ST-LINK_CLI.exe too...

A1bucker by Associate III
  • 1233 Views
  • 1 replies
  • 0 kudos

Resolved! Putting STM32F103 in sleep mode

Hello,I am trying to put my STM32F103C8T8 in sleep mode where all clocks are running etc. and wake it up using external UART interrupt.I am using MikroC as an environment and I don't think they have Wait for interrupt function. Is there any other sol...

UMilo.1 by Associate III
  • 6460 Views
  • 7 replies
  • 2 kudos

Package Data Register

I am using 2 devicesSTM32L4A6VGY6P (package WLCSP100L) STM32L4A6ZGT6P (package LQFP144)My FW needs to differentiate between these 2 devices and so the package data register (0x1FFF7500) seems like a no brainer to use for that.The problem is my WLCSP1...

MCUExpert_0-1691213163624.png
MCUExpert by Associate II
  • 1660 Views
  • 4 replies
  • 0 kudos

STM32WB55 Code is stuck in HAL_Delay() function

Hello ,   I am searching for solution that my code is stuck in the hal_delay function. I couldnt figure it out exact solution. Indeed, this problem is posted in community many times. When I try to initilize the code form cubeMX and test it on --nucle...

baydı.1 by Associate III
  • 1866 Views
  • 1 replies
  • 0 kudos

General information about FDU?

Hello, Our goal is to implement field firmware updates in our application and would like to gain a general understanding of how it works at ST.From reading the Application note: STM32 microcontroller system memory boot mode, my understanding is that ...

ewilliams by Associate II
  • 3370 Views
  • 4 replies
  • 2 kudos

STM32H747 SPI1 not working

I tryed to working SPI1 of stm32h747. But I seen jast 8 clock signag on the sck. after that signal is down. İ didn't find the reason. There is available how mate setup code an signal pohotograf. void MX_SPI1_Init(void){/* USER CODE BEGIN SPI1_Init 0 ...

Snm.1 by Associate III
  • 1520 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.