STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Write variables into non-voaltive memory STM32L010K8T6TR

Hi, I need to write a variable, like ID , for a new design.This ID during the normal program execution the user can change in order to assing a new ID. In the next re-start this new ID must to be can read.someone could me help to implement this funct...

loopis80 by Associate
  • 1856 Views
  • 3 replies
  • 0 kudos

STM32H7 pin related query

Hi,I am using STM32H743ZIT6 in my design but due to the availability issue I am planning to use STM32H723ZGT6 as it is a P2P compatible.I have the below queries related to the UART and SPI:For UART :Can RS485 be used with USART ?For debug UART3 in 72...

Sandeep1 by Associate II
  • 3213 Views
  • 5 replies
  • 0 kudos

Resolved! Define ISR as weak using CubeMX LL Drivers

Hello,For efficiency reason I need to use only the LL, so I enable the LL flag in the CUBEMX configuration.I would like to have the ISR defined as __weak, so that I can write my own version without replacing manually the ISR.I know that using HAL dri...

w25q128jv

I want to read and write to w25q128jv with stm32l5 octo spi insted of quad spi.. is there anybody help me. ı could not write correctly.. and ı could not erase. correctly. first problem is when ı was write whiel start addres 0 my code write start to t...

Snm.1 by Associate III
  • 11727 Views
  • 10 replies
  • 4 kudos

Touch GFX Two Layers frame buffer update issue

Hi,In TouchGFXGeneratedHAL.CPP u are using the HAL_LTDC_LineEventCallback. the issue is i use the two layers.Layer_1 for live video from camera and layer_2 for GUI. every time i generate code i must add this code below. the added code in bold,italic....

MSale.1 by Senior
  • 933 Views
  • 0 replies
  • 0 kudos

UART COM issue with f030r8

Hello,I am trying to use UART HAL with the stm32-f030r8 connected to the PC through a USB-TTL module.The configuration is given below :- The F030R8 has JP1 OFF, JP6 ON, JP5 on E5V.- The USB-TTL is :- The code is :/* Includes -------------------------...

wire.PNG usb-ttl.jpg
user-stm by Associate II
  • 7656 Views
  • 12 replies
  • 0 kudos

Resolved! Boot0 Pin issue in STM32L051

What would happen to the microcontroller if during running normally then suddenly the boot_0 pin switched to high?in my case and due some voltage spike the boot_0 pin state switched to high for very short time nano seconds. most of the time its ok bu...

MSale.1 by Senior
  • 3249 Views
  • 2 replies
  • 0 kudos

Resolved! QSPI Initialization AutoPolling timeout without BSP

Working with the STM32H747i-Eval board with a touchGFX application. Need the QSPI for assets and not wanting to use the BSP due to wanting to have more control over clock speeds and pinout configuration.I'm in need of some more experienced advice whe...

Resolved! Release Firmware vs. Debug Firmware Behaving Differently

I have noticed lately that when switching between my release and debug build configurations that the code behaves differently. Looking at the Project Build Settings the only difference I see between the two is the Release GCC and G++ compilers are op...

Jaboop by Associate II
  • 4137 Views
  • 3 replies
  • 3 kudos

DMA Mode change source Increment address

ILI9341 SPI display running on an L5 processor on a custom board.In a never ending quest to make the display go faster, I've split off the generic write image from the generic fill block.Since the high level drivers work with any type of display, all...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.