STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SD Write error some time , not stable

Hi ,   I made a STM32F405VGT6 board with SD card interface. The SD code is generated using STM32CUBEMX and FatFs middleware.   The SD file write is not stable, it return error sometimes after calling f_write(). However, if I run the same code in uVis...

MHo.15 by Associate III
  • 5795 Views
  • 5 replies
  • 0 kudos

Placing variables in dedicated part of memory.

Hi  I'm using a STM32L433 in a battery application, and running in Stop mode. I want to keep some variables in RAM2 so their values are not lost when the processor is woken up.I managed to get it working as follows. I created a block in the linker fi...

Resolved! NUCLEO-H723ZG I2S with PI-mod i2s stereo codec

Hey everyoneI was successfully running i2s on the stm m4 cores but trying to make the jump to h7 and running into a issue. Using the same code and the DMA triggers but no code is being loaded in the rx buffer. Not sure the tx buffer is being sent out...

stm32L073 Flashing

I am using STM32L073RZI MCU on a custom PCB design. I am looking for a board that flashes the chip before I place it on the PCB.  I checked st.com website and I didn't see any product to flash the chip. Is there any board to flash the firmware onto t...

oucler by Associate II
  • 2735 Views
  • 4 replies
  • 3 kudos

STEVAL-ESC001V1 CAN interface

I am looking for information regarding the CAN interface on the STEVAL-ESC001v1 board. In the features of the device it lists CAN as a feature but the documentation does not provide additional information on how exactly the CAN interface can be used ...

High Current on Nucleo H745ZI-Q in Standby Mode

Hello all,I am evaluating the STM32H745 for an application which requires very low power. I am using the Nucleo H745ZI-Q for this evaluation and STM example code I downloaded. The datasheet for the STM32H745 indicates that I should expect to see a cu...

USART1 interrupt handler not called

Hello,first, I'm new to STM32 Nucleo MCUs, so if I am asking something that is well-known in documentation of Nucelo boards please advise me to correct documentation.I have a project using a STM32 L432KC that gets serial data from another MCU and sen...

lorky by Associate
  • 15502 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.